The following steps allow you to build a bootable image in two different ways and also how to enable and use SCFW debug monitor. There are four files needed to generate a bootable image:
├── bl31.bin
├── u-boot.bin
├── mx8qm-ahab-container.img
└── scfw_tcm.bin
There are some ways to get the four files, one way is with Yocto and other way is with stand alone build.
To get the four files needed with Yocto, you have to build an i.MX 8QuadMax image, maybe some steps are not necessary.
sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib \
build-essential chrpath socat cpio python python3 python3-pip python3-pexpect \ xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa \
libsdl1.2-dev pylint3 xterm rsync curl
mkdir ~/bin (this step may not be needed if the bin folder already exists)
curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
export PATH=~/bin:$PATH
git config --global user.name "Your Name"
git config --global user.email "Your Email"
git config --list
mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-hardknott -m imx-5.10.72-2.2.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8qmmek source imx-setup-release.sh -b imx8qmmek
bitbake imx-image-full
The four files needed to generate a bootable image are in:
~/imx-yocto-bsp/imx8qmmek/tmp/deploy/images/imx8qmmek/imx-boot-tools
Note: With Yocto you can not enable the SCFW debug monitor.
For more information see the i.MX Yocto Project User's Guide.
To build all required binaries from source you can use standard aarch64 Linux toolchain, on Ubuntu 20.04 LTS:
sudo apt-get install gcc-aarch64-linux-gnu
Download source from:
git clone -b lf-5.10.72-2.2.0 https://source.codeaurora.org/external/imx/imx-atf
Build:
cd imx-atf
make clean PLAT=imx8qm CROSS_COMPILE=aarch64-linux-gnu-
make PLAT=imx8qm CROSS_COMPILE=aarch64-linux-gnu- bl31
The compiled bl31.bin location:
build/imx8qm/release/bl31.bin
Download source from:
git clone -b lf-5.10.72-2.2.0 https://source.codeaurora.org/external/imx/uboot-imx
Build:
cd uboot-imx
make ARCH=arm CROSS_COMPILE=aarch64-linux-gnu- imx8qm_mek_defconfig
make ARCH=arm CROSS_COMPILE=aarch64-linux-gnu-
The compiled u-boot.bin location:
./u-boot.bin
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-seco-3.7.4.bin
chmod +x imx-seco-3.7.4.bin
./imx-seco-3.7.4.bin --auto-accept
The mx8qmb0-ahab-container.img file location:
imx-seco-3.7.4/firmware/seco/mx8qmb0-ahab-container.img
Look at the packages/imx-scfw-porting-kit-1.7.4/doc/pdf/, chapter Porting Guide, sub-chapter Tool Chain to check which GNU Toolchain version corresponds to the SCFW you are building. The imx-scfw-porting-kit-1.7.4 version uses the GNU Toolchain version gcc-arm-none-eabi-8-2018-q4-major. It is recommended to install toolchain in “opt” folder:
cd /opt
sudo wget https://developer.arm.com/-/media/Files/downloads/gnu-rm/8-2018q4/gcc-arm-none-eabi-8-2018-q4-major-linux.tar.bz2
sudo tar xjf gcc-arm-none-eabi-8-2018-q4-major-linux.tar.bz2
It is recommended to install toolchain in “opt” folder:
sudo wget https://releases.linaro.org/components/toolchain/binaries/7.3-2018.05/aarch64-linux-gnu/gcc-linaro-7.3.1-2018.05-x86_64_aarch64-linux-gnu.tar.xz
sudo tar -Jxvf gcc-linaro-7.3.1-2018.05-x86_64_aarch64-linux-gnu.tar.xz
After installing the toolchain, set up the environment variable relevant for building.
export ARCH=arm
CROSS_COMPILE=/opt/gcc-linaro-7.3.1-2018.05-x86_64_aarch64-linux-gnu/bin/aarch64-linux-gnu-
export TOOLS=/opt
cd ~
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-scfw-porting-kit-1.7.4.bin
chmod +x imx-scfw-porting-kit-1.7.4.bin
./imx-scfw-porting-kit-1.7.4.bin --auto-accept
cd imx-scfw-porting-kit-1.7.4/src
Extract the desired scfw porting kit:
tar -xvf scfw_export_mx8qm_b0.tar.gz
cd scfw_export_mx8qm_b0/
Build without debug monitor:
make clean
make qm B=mek R=B0
Build with debug monitor:
make clean
make qm B=mek D=1 M=1 R=B0 DDR_CON=imx8qm_dcd_1.6GHz
The scfw_tcm.bin file location:
build_mx8qm_b0/scfw_tcm.bin
Once you have the four files needed to generate a bootable image, use imx-mkimage tool.
Download source from:
git clone -b lf-5.10.72-2.2.0 https://source.codeaurora.org/external/imx/imx-mkimage
You have to rename some files.
cp ~/imx-yocto-bsp/imx8qmmek/tmp/deploy/images/imx8qmmek/imx-boot-tools/bl31-imx8qm.bin ~/imx-mkimage/iMX8QM/bl31.bin
cp ~/imx-yocto-bsp/imx8qmmek/tmp/deploy/images/imx8qmmek/imx-boot-tools/u-boot-imx8qmmek.bin-sd ~/imx-mkimage/iMX8QM/u-boot.bin
cp ~/imx-yocto-bsp/imx8qmmek/tmp/deploy/images/imx8qmmek/imx-boot-tools/mx8qmb0-ahab-container.img ~/imx-mkimage/iMX8QM
cp ~/imx-yocto-bsp/imx8qmmek/tmp/deploy/images/imx8qmmek/imx-boot-tools/mx8qm-mek-scfw-tcm.bin ~/imx-mkimage/iMX8QM/scfw_tcm.bin
cp ~/imx-atf/build/imx8qm/release/bl31.bin ~/imx-mkimage/iMX8QM
cp ~/uboot-imx/u-boot.bin ~/imx-mkimage/iMX8QM
cp ~/imx-seco-3.7.4/firmware/seco/mx8qmb0-ahab-container.img ~/imx-mkimage/iMX8QM
cp ~/imx-scfw-porting-kit-1.7.4/src/scfw_export_mx8qm_b0/build_mx8qm_b0/scfw_tcm.bin ~/imx-mkimage/iMX8QM
cd ~/imx-mkimage
make SOC=iMX8QM flash
The compiled file is flash.bin and its location is:
iMX8QM/flash.bin
To flash the bootable image follow the next steps:
-Copy the flash.bin and uuu.exe in a folder.
-Change SW2 on the base board to 000100 (from MSB to LSB, 1-ON and 0-OFF) to boot from the Serial Downloader.
-Run the following command in Command Prompt:
uuu.exe -b sd flash.bin
-Power on the MEK CPU board.
If the SCFW is compiled using the M=1 option (default is M=0) then it will include a debug monitor. This can be used to R/W memory or registers, R/W power state, and dump some resource manager state. Production SCFW should never have the monitor enabled (M=0, the default)!
The debug monitor allows command-line interaction via the SCU UART. Inclusion of the debug monitor affects SCFW timing and therefore should never be deployed in a product! Note the terminal needs to be in a mode that sends CR or LF for a new line (not CR+LF).
The following commands are supported:
Command Description
exit exit the debug monitor
quit exit the debug monitor
reset [mode] request reset with mode (default = board)
reboot partition [type] request partition reboot with type (default = cold)
md.b address [count] display count bytes at address
md.w address [count] display count words at address
md[.l] address [count] display count long-words at address
mm.b address value modify byte at address
mm.w address value modify word at address
mm[.l] address value modify long-word at address
ai.r ss sel addr read analog interface (AI) register
ai.w ss sel addr data write analog interface (AI) register
fuse.r word read OTP fuse word
fuse.w word value write value to OTP fuse word
dump rm dump all the resource manager (RM) info
dump rm part [part] dump all partition info for part (default = all)
dump rm rsrc [part] dump all resource info for part (default = all)
dump rm mem [part] dump all memory info for part (default = all)
dump rm pad [part] dump all pad info for part (default = all)
power.r [resource] read/get power mode of resource (default = all)
power.w resource mode write/set power mode of resource to mode (off, stby, lp, on)
info display SCFW/SoC info like unique ID, etc.
seco lifecycle change send SECO lifecycle update command (change) to SECO
seco info display SECO info like Lifecycle, SNVS state, etc.
seco debug dump SECO debug log
seco events dump SECO event log
seco commit commit SRK and/or SECO FW version update
pmic.r id reg read pmic register
pmic.w id reg val write pmic register
pmic.l id list pmic info (rail voltages, etc)
Resource and subsystem (ss) arguments are specified by name. All numeric arguments are decimal unless prefixed with 0x (for hex) or 0 (for octal).
-Change SW2 on the base board to 001100 (from MSB to LSB, 1-ON and 0-OFF) to boot from the SD card.
-Power on the MEK CPU board.
-Open Tera Term and you will see:
Hello from SCU (Build 5263, Commit 9b3d006e, Aug 20 2021 12:20:10)
DDR frequency = 1596000000
ROM boot time = 262368 usec
Boot time = 24583 usec
Banner = 10 usec
Init = 9038 usec
Config = 3232 usec
DDR = 2677 usec
SConfig = 444 usec
Prep = 5039 usec
*** Debug Monitor ***
>$
-Run the following commands:
power.r
power.w db on
power.w dblogic on
power.w mu_1a on
-Example reading on Linux side:
md.l 0x5d1c0000 10
-You will see:
>$ md.l 0x5d1c0000 10
5d1c0000: 00000000 00000000 00000000 00000000
5d1c0010: 00010201 23c34600 d63fdb21 00000000
5d1c0020: 00f00200 18000000
-Example reading on SCU side:
md.l 0x41cac080 10
-You will see:
>$ md.l 0x41cac080 10
41cac080: 00000000 00000000 00000000 00000000
41cac090: 0d070201 ff0001f1 ffff8000 ffff00fb
41cac0a0: 00f00000 18000000
For more information see the System Controller Firmware Porting Guide.