This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board.
A) Basic Requirement:
B) Installed the needed packages to the Linux Host PC
$ sudo apt-get update
$ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev
$ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool
$ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool
$ sudo apt-get install uuid-dev liblzo2-dev
$ sudo apt-get install tcl dpkg
$ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev
$ sudo apt-get install texlive texinfo
$ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1
$ sudo apt-get install uboot-mkimage
$ sudo apt-get install scrollkeeper
$ sudo apt-get install gparted
$ sudo apt-get install nfs-common nfs-kernel-server
$ sudo apt-get install git-core git-doc git-email git-gui gitk
$ sudo apt-get install meld atftpd
C) Unpack and install the LTIB source package and assume done on the home directory:
$ cd ~
$ tar -zxvf L3.0.35_4.1.0_130816_source.tar.gz
$ ./L3.0.35_4.1.0_130816_source/install
After that, you will find ~/ltib directory created
D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS
$ cd ~/ltib
$ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_12.04_64bit_OS.patch
The patch modifies the following files:
E) Then, it is ready to proceed the rest of the LTIB env setup process:
$ cd ~/ltib
$ ./ltib -m config
$ ./ltib
Reference:
NOTE:
When compiling gstreamer, this warning was pop up. Just ignore it seems okay.
Do you still need first 2 patches mentioned in answer to one of your references: https://community.freescale.com/message/332385#332385?
1) install patch-ltib-ubuntu12.04.sh from (https://community.freescale.com/docs/DOC-93455).
2) create a soft link under /usr/include.
sudo ln -s i386-linux-gun/sys sys