Prerequisites:
The build is verified on prebuilt rootfs(based on LTIB) which can be downloaded from freescale.com
EGL uses framebuffer backend
libEGL.so -> libEGL-fb.so
libGAL.so -> libGAL-fb.so
QT4.8
1. Download the git respository for qt4.8:
$ git clone http://git.gitorious.org/qt/qt.git qt
$ cd qt
Let us consider this as <QTDir>
2. Create /tftpboot and point your target fileystem. As like
$ mkdir -p /tftpboot
$ cd /tftpboot
$ ln -s $(ROOTFFS) rootfs
TBD:Need to work on this to use sysroot option
3. Create a build directory to install for the qt4 packages. This directory can be in any location. For example,
$ mkdir /opt/qt4
$ sudo chown -R <username> /opt/qt4
Let us consider the the <installdir> as /opt/qt4
4. Extract the attached mkspecs(linux-imx6-g++.tar.gz) to <QTDir>/mkspecs/qws/
5. Apply the attached cd 0001-add-i.MX6-EGL-support.patch attached to enable egl support for i.MX6
$ cd <QTDir>
$ patch -p1<0001-add-i.MX6-EGL-support.patch
6. Export CROSS-COMPILE location path to PATH
$ export PATH=$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/
7. Enter to the <QTDir>. Do configure. You can select the options as you like. Here is an example
$ cd <QTDir>
$ ./configure -qpa -arch arm -xplatform qws/linux-imx6-g++ -no-largefile -no-accessibility \
-opensource -verbose -system-libpng -system-libjpeg -system-freetype -fast -opengl es2 -egl -confirm-license \
-qt-zlib -qt-libpng -no-webkit -no-multimedia \
-make examples -make demos \
-release -make libs -exceptions -no-qt3support -prefix <installdir>
8. When the configure summary is shown make sure the Qt has OpenGL ES 2.0 support. Do build
$ make
$ make install
9. Now need to build eglfs plugin
$ cd <QTDir>/src/plugins/platforms/eglfs
$ make
$ make install
Now the eglfs will be installed to the QT Install directory.
10. By now all required QT files are in <install directory>
11. Copy the install directory to target filesystem
$ cp -rf /opt/qt4 /tftpboot/rootfs/opt/.
12. Running Qt apps on target
- Boot the target either with NFS or SD Image
- Ensure that folder <installdir> is copied on target file system at “/usr/local”.
- Launch application using
$ cd /opt/qt4/examples/opengl/hellogl_es2
$ ./hellogl_es2 -platform eglfs
QT5
These steps are performed on the host
1. Download the git respository for qt5:
$ git clone git://gitorious.org/qt/qt5.git qt5
$ cd qt5
Let us consider this as <QTDir>
2. Create a build directory to install for the qt5 packages. This directory can be in any loctation. For example,
$ sudo mkdir /opt/qt5
$ sudo chown -R <username> /opt/qt5
Let us consider the the installdir as /opt/qt5
3. Enter the Qt5 directory and run the init-repository script to download all the source code for
Qt5. To download all the source code will take about an hour.
$ ./init-repository
Update: In the latest Qt5 release the webkit library is included by default and there are some issues trying to compile it.
use the next line to avoid problems if not desired to use webkit.
$ ./init-repository --no-webkit
4. From the following path
$ gedit qtbase/mkspecs/devices/linux-imx6-g++/qmake.conf
5. At the top of the qmake.conf, there is a configure line. Copy and paste the configure line into a text file located
in your build build directory. Edit the configure line to find your toolchain and filesystem. Also make sure to
include the options -no-pch, -no-opengl, -opengl es2, Here is an example of
a configure line.
Update: In the latest Qt5 stable, the option to compile the examples/demos is -compile-examples, instead of -make examples -make demos
If you are running into problems with webkit, use the option -no-icu, this will disable the webkit.
$ cd <QTDir>
$ cd qtbase
$ ./configure -v -opensource -confirm-license -no-pch -no-xcb -no-opengl -opengl es2 \
-make libs -device imx6 \
-compile-examples \
-device-option CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi- \
-sysroot <rootfs> -no-gcc-sysroot \
-prefix <installdir>
7. Make the textfile that has the configure line and executable and run it. When the configure summary is shown make sure the Qt5 has openGL ES 2.0 support. Do build
$ make
$ sudo make install
When Qt5 has finished building, Qt5 will be installed in two places:
1. <location of rootfs>/<installdir>
2. <HOST Machine>/<install dir>
This is good because now all the libraries and binaries for Qt5 are installed on the host and the target filesystem. Therefore, the target already has all the libraries and binaries needed to run Qt5.
8. Also need to build qtjsbackend and qtdeclarative.
$ cd <location to Qt5 git>
$ cd qtjsbackend
$ ../qtbase/bin/qmake -r
$ make && sudo make install$ cd <location to Qt5 git>
$ cd qtdeclarative
$ ../qtbase/bin/qmake -r
$ make && sudo sudo make install
9. Running Qt apps on target
- Boot the target either with NFS or SD Image
- Ensure that folder <installdir> is copied on target file system at “/usr/local”.
- Launch application using
$ cd /opt/qt5/examples/opengl/hellowindow
$ ./hellowindow -platform eglfs
FAQ:
On the target file system, the location of target libaries and includes may present in arm-linux-gnueabi directory. Make sure to create soflinks to QT can find. For example
$ cd $(ROOTFS)/usr/lib
$ ln -s arm-linux-gnueabi/libffi.so.6 libffi.so.6
While building QT5, you may see a build error that libQt5V8.so.5 is not found. This might be some problem to be addressed in QT. Workaround is to
copy all the binaries to correct path as like this
$ cp <ROOTFS>/<installdir>/lib/* <HOST Machine>/<installdir>/.
What is coming up next:
1. QT on X is already available on Yocto filesystem. Steps to enable GPU Acceleration TDB.
2. QT with Wayland support.
First: I'm a very beginner in developing software for Linux Embedded. So may be my questions
are very basic. I'm sorry for that.
I need to cross-compile a QT 5 program from a PC based Ubuntu system to a i.MX6 board.
I already built the O.S. for the board following the instructions of the page
"https://github.com/Freescale/fsl-community-bsp-platform".
Now I'm trying to set up QT following the
https://community.freescale.com/docs/DOC-94066
document, i.e. this page.
I did step 1, 2, 3 and 4.
At step 5 gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 is referenced.
Where can I find it?
I looked for it on http://www.linaro.org/ site but I didn't find it.
Thanks!
As I noticed that there is a patch file 0001-add-i.MX6-EGL-support.patch for Qt 4.8, however, there is not such a patch for QT5.
Did you miss it? There might be a similar patch to Qt5.
As I tried the hellowindow application in Qt 5.1, I got error log as follow. Do you have any hints?
</opengl/hellowindow$ ./hellowindow -platform eglfs
QIconvCodec::convertFromUnicode: using Latin-1 for conversion, iconv_open failed
QIconvCodec::convertToUnicode: using Latin-1 for conversion, iconv_open failed
QEglFSImx6Hooks will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.
If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
EGLFS: Unable to query physical screen size, defaulting to 100 dpi.
EGLFS: To override, set QT_QPA_EGLFS_PHYSICAL_WIDTH and QT_QPA_EGLFS_PHYSICAL_HEIGHT (in millimeters).
EGLFS: OpenGL windows cannot be mixed with others.
Aborted
Hi, xicai chen.
I have the same problem with hellowindow application in Qt 5 (EGLFS: OpenGL windows cannot be mixed with others)
You solved it?
I would suggest everyone who uses already YOCTO for their images to also use it to compile Qt
See for a working Qt5 tutorial here:
Everyone who doesn't use YOCTO not 'til now: DO IT :smileygrin: read more about it in the Yocto Training - HOME
If you want to use Qt4, you can do this even easier because of the different layers that YOCTO delivers...
for the board: qt-in-use-image or qte-in-use-image
as toolchain: meta-toolchain-qt or meta-toolchain-qte
Have fun!
Hello Bradley,
I'm starting with IMX6 and Qt.
I followed the instructions but I'm having the same issue as yours. I have the same directories after the install, nothing more, and some errors during "make" and "make install".
Did you find a solution to build Qt4.8 for the IMX6?
Nicolas
Hey I am experimenting with Yocto and my Mx6 Board. I am using dora and I used qte-in-use-image to "bake" an image. I want to experiment with QT + OpenGL using the framebuffer.
I disable X11 and Wayland with the flag: DISTRO_FEATURES_remove = "x11 wayland" on my local.conf
I am able to run the vivante vdk examples but I have not being able to run the hellogl_es2 example from OpenGL. I get a pitch black rendering. Have you being able to run the OpenGL examples from QT?
AFAIK the qt-in-use-image only produces a rootfs for Qt 4.8 - but still the version should be good enough to compile the hellogl_es2 example.
I tried to compile the application with my Qt 5.1.1 toolchain (see link in my previous comment) but it didn't work - gnu/stubs-soft.h wasn't found... I didn't recognize this error before and don't know how to handle this - so sorry, I cant help you with that :smileysad:
I found out that the hellogl_es2 example is not able to run when you dont have X11 or wayland. You need a windowing system because the hellogl_es2 encapsulates an QGLWidget within another widget. Better is to use QT5 + QML. I will give it a try. And probably your error is because you have to edit the file qtbase/mkspecs/devices/linux-imx6-g++/qmake.conf and add -mfloat-abi=hard in IMX6_CFLAGS. Give it a try.
Hey,
I successfully installed qt 4.8 in my target.
Initially i had 4.6.0 on my target, which had audio demo codes. 4.8 doesn't seem to have any multimedia demos. The existing examples execute correctly. however any example which i used to
run in 4.6.0 using qws doesn't seem to execute on 4.8. It crashes with a "segmentation fault".
I have qtCreater 2.7.2 with Qt 4.8.4 on my host, and any example code for instance a system call code or a mmap call doesn't seem to work.
I had shifted to 4.8 assuming and expecting better audio and Serial communication support. but simple codes compiled do not work in ltib. It is very frustrating.
Can anyone please help me out with that.
regards,
nishad
I am trying to setup a cross compiler setup for the RIOT (IMX6) on opensuse 13.21 (64), as I would like to use qt with qws under Ubuntu Image (Must still figure out how-to disable the GUI, as this is not a 'standard' Unbuntu startup)
Step 6 assumes one has a cross compiler already installed.
export PATH=$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/
How can I install this, where can I download it, as it seem to 'included' in some BSD package.
Thanks
I'm building qt-5.1.1 from dora branch of yocto project. All fine works instead HTML5 video from simple browser in qtwebkit-examples
I see player controls, but it doesn't work. On some videos i can view freeze frame of videos, but it not playing.
In console gstreamer output messages like this:
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
libpng warning: iCCP: Not recognizing known sRGB profile that has been edited
Received finished signal while progress is still: 10 Url: QUrl( "http://qt-project.org/" )
Aiur: 3.0.11
Core: MPEG4PARSER_06.07.04 build on Dec 5 2013 11:41:38
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2
Content Info:
URI:
https://r1---sn-8xb5-px8e.googlevideo.com/videoplayback?ip=212.90.165.14&require
ssl=yes&mws=yes&source=youtube&upn=4-tA0Ie6tDA&mv=m&sparams=id,ip,ipbits,itag,ra
tebypass,requiressl,source,upn,expire&key=yt5&ipbits=0&mt=1401803916&id=o-ABczKx
qqFwtM_XhBgSvGnsGqyiHL18Wy6SqK0BZepcFQ&signature=121A2CB3142FB772CD72A9F1D872603
C749A2B74.0370EDFC498A96A43C8F8A98C10184E14158A0D2&sver=3&ratebypass=yes&expire=
1401827798&ms=au&fexp=908548,912321,913434,916611,923341,926122,930008&itag=18&c
pn=VgAqvxj2iI2hp45w&ptk=youtube_none&pltype=contentugc&c=WEB&cver=html5
Seekable : Yes
Size(byte): 32830110
Movie Info:
Seekable : Yes
Live : No
Duration : 0:11:52.503360000
ReadMode : Track
Track : 2
Track 00 [video_000000] Enabled
Duration: 0:11:52.503360000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, width=(int)640, height=(int)360, framerate=(
fraction)24000/1001
Track 01 [audio_000000] Enabled
Duration: 0:11:52.503360000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)9
6000, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)121000
00000000000000000000000000
Beep: 3.0.11
Core: AAC decoder Wrapper build on Jan 22 2014 15:42:53
mime: audio/mpeg, mpegversion=(int){2,4}
file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm12_elinux.so.3
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.07.00_CORTEX-A8 build on Sep 18 2013 10:29:53.
[--->FINALIZE aiurdemux
QtMultimedia examples working correctly.
Whats wrong and how can I fix it?
Hi all, i'm trying to build qt5 for a udoo quad board (use imx6 quad http://www.udoo.org/) but i'm blocked at ./configure. i had some errors :
/home/modjo/Udoo/Qt5_build/fsl-linaro-toolchain/arm-fsl-linux-gnueabi/bin/g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp -g -Wall -W -fPIE -I../../mkspecs/devices/linux-imx6-g++ -I. -I../../../../usr/include -I../../../../usr/bin -o arch.o arch.cpp
g++: error trying to exec 'cc1plus': execvp: No such file or directory
Messages de l'assembleur:
Erreur fatale: option -march= invalide: « armv7-a »
gmake: *** [arch.o] Erreur 1
Unable to determine architecture!
Could not determine the target architecture!
Turn on verbose messaging (-v) to see the final report.
Determining architecture... ()
g++ -c -pipe -g -Wall -W -fPIE -I../../mkspecs/linux-g++ -I. -o arch.o arch.cpp
g++ -o arch arch.o
Found architecture in binary
CFG_HOST_ARCH="i386"
CFG_HOST_CPUFEATURES=""
System architecture: 'unknown'
Host architecture: 'i386'
C++11 auto-detection... ()
/home/modjo/Udoo/Qt5_build/fsl-linaro-toolchain/arm-fsl-linux-gnueabi/bin/g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp -O2 -std=c++0x -Wall -W -fPIE -I../../../mkspecs/devices/linux-imx6-g++ -I. -I/home/modjo/Udoo/Qt5_build/usr/include -I/home/modjo/Udoo/Qt5_build/usr/bin -o c++11.o c++11.cpp
g++: error trying to exec 'cc1plus': execvp: No such file or directory
Messages de l'assembleur:
Erreur fatale: option -march= invalide: « armv7-a »
gmake: *** [c++11.o] Erreur 1
C++11 disabled.
.......
......
......
......
OpenGL ES 2.x auto-detection... ()
/home/modjo/Udoo/Qt5_build/fsl-linaro-toolchain/arm-fsl-linux-gnueabi/bin/g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp -O2 -Wall -W -fPIE -I../../../mkspecs/devices/linux-imx6-g++ -I. -I/home/modjo/Udoo/Qt5_build/usr/include/GLES2 -I/home/modjo/Udoo/Qt5_build/usr/include -I/home/modjo/Udoo/Qt5_build/usr/bin -o opengles2.o opengles2.cpp
g++: error trying to exec 'cc1plus': execvp: No such file or directory
Messages de l'assembleur:
Erreur fatale: option -march= invalide: « armv7-a »
gmake: *** [opengles2.o] Erreur 1
OpenGL ES 2.x disabled.
The OpenGL ES 2.0 functionality test failed!
You might need to modify the include and library search paths by editing
QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in
/home/modjo/Udoo/Qt5_build/qt5/qtbase/mkspecs/devices/linux-imx6-g++.
For information the Udoobuntu file system : http://www.udoo.org/downloads/
the link for the tutorial : http://www.udoo.org/ProjectsAndTutorials/how-to-build-qt5-for-udoo/?portfolioID=1394
my qmake.conf :
include(../common/linux_device_pre.conf)
ROOTFS_PATH=/home/modjo/Udoo/Qt5_build
TOOLCHAIN_PREFIX=/home/modjo/Udoo/Qt5_build/fsl-linaro-toolchain/arm-fsl-linux-gnueabi/bin
EGLFS_PLATFORM_HOOKS_SOURCES = $$PWD/qeglfshooks_imx6.cpp
QMAKE_INCDIR += $${ROOTFS_PATH}/usr/include $${ROOTFS_PATH}/usr/bin
QMAKE_LIBDIR += $${ROOTFS_PATH}/usr/lib/arm-linux-gnueabihf $${ROOTFS_PATH}/usr/lib
QMAKE_INCDIR_OPENGL_ES2 += /home/modjo/Udoo/Qt5_build/usr/include/GLES2
QMAKE_LIBDIR_OPENGL_ES2 += /home/modjo/Udoo/Qt5_build/usr/lib/GLESv2
#QMAKE_LIBS_EGL += /home/modjo/Udoo/Qt5_build/usr/lib/GLESv2
#QMAKE_LIBS_OPENGL_ES2 += /home/modjo/Udoo/Qt5_build/usr/lib/GLESv2
#QMAKE_LIBS_OPENVG += /home/modjo/Udoo/Qt5_build/usr/lib/OpenVG
QMAKE_LIBS_EGL += -lEGL
QMAKE_LIBS_OPENGL_ES2 += -lGLESv2 -lEGL -lGAL
QMAKE_LIBS_OPENVG += -lOpenVG -lEGL -lGAL
QMAKE_LFLAGS += -Wl,-rpath-link,$$/home/modjo/Udoo/Qt5_build/lib/arm-linux-gnueabihf
IMX6_CFLAGS = -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1
QMAKE_CFLAGS += $$IMX6_CFLAGS
QMAKE_CXXFLAGS += $$IMX6_CFLAGS
include(../common/linux_arm_device_post.conf)
load(qt_config)
and my configure :
./configure -prefix /opt/qt5 -make libs -no-pch -no-opengl -device imx6 -device-option CROSS_COMPILE=/home/modjo/Udoo/Qt5_build/fsl-linaro-toolchain/arm-fsl-linux-gnueabi/bin/ -no-largefile -opengl es2 -qt-zlib -qt-libpng -qt-libjpeg -no-nis -no-cups -gui -make examples -sysroot /home/modjo/Udoo/Qt5_build/exemples -no-gcc-sysroot -opensource -confirm-license -qreal float -v
Do you an idea to resolve this ?
Hi ,
I successfully cross compiled QT5 for my custom iMX6Q board,
I used LTIB 3.0.35_4.1.0 kernel for building my u-boot, kernel and rootfs.
I am attaching documents and links that i prepared to help anyone who
wishes to build QT5, it might not help you directly, but the procedure
should help you.
regards,
Nishad
Ok nishad, i'm waiting for your procedure ! thank's in advance !
Configuration Script:
./configure -v -opensource -confirm-license -no-sse2 -no-sse3 -no-ssse3
-no-sse4.1 -no-sse4.2 -no-avx -no-xcb -no-sql-mysql -no-sql-db2
-no-sql-ibase -no-sql-oci -no-sql-odbc -no-sql-tds -no-sql-sqlite2
-no-pch -no-opengl -opengl es2 -wayland -make libs -device imx6 -make
examples -device-option
CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-
-sysroot /home/sumeet/ltib/rootfs -no-gcc-sysroot -prefix /usr/local/QT_5
Link to be followed thoughtfully along with the procedure given on the
current link above:
http://qt-project.org/wiki/RaspberryPi_Beginners_guide
I used the "cross-compiled-tools" to compile QT-5
and built individual modules using the link.
you need to download it as use it taking reference of the script given below for setting up path.
Cleaning a_config_if_compile_wrong:
sudo git submodule foreach --recursive "git clean -dfx"
Script for_setting_paths:
./fixQualifiedLibraryPaths /home/sumeet/ltib/rootfs
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-g++
You might get fontconfig errors, which you need to solve by analysing
the error.
Although i was able to install QT5 , i still have problems with fonts, i
am not able to see fonts in the GUI. i am working on it.
regards
nishad
Hi all,
I tried build qt5 like in this doc.
My configuration command is:
./configure -v -opensource -confirm-license -make libs -device imx6 -device-option CROSS_COMPILE=/home/x0158990/hdd/tools/poky/1.7/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi- -sysroot /home/x0158990/hdd/tools/poky/1.7/sysroots/x86_64-pokysdk-linux -no-gcc-sysroot -prefix /home/x0158990/work/tools/QT5
I have got error:
Precompiled-headers support enabled.
/home/x0158990/hdd/tools/poky/1.7/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++ -c -fvisibility=hidden fvisibility.c
Symbol visibility control enabled.
/home/x0158990/hdd/tools/poky/1.7/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++ -o libtest.so -shared -Wl,-Bsymbolic-functions -fPIC bsymbolic_functions.c
bsymbolic_functions.c:2:2: error: #error "Symbolic function binding on this architecture may be broken, disabling it (see QTBUG-36129)."
#error "Symbolic function binding on this architecture may be broken, disabling it (see QTBUG-36129)."
^
Symbolic function binding disabled.
In QTBUG-36129 bug's description I didn't found applicable solution.
Please help!
HI nice tutorial.... can you pls give some insights about qt webkit as well how to render a fullscreen HTML5 based webpage using that... am really new to qt... pls guide me
Hi,
I have successfully build Qt4.8 for imx6. But when I tried to run the sample example I got the below error:
"Could not create the egl surface: error = 0x300b"
Please help me out of this.
Regards,
Paritosh
Hi,
Sorry for the delay in reply,
Could you give me more information about your problem?
Are you using LTIB to build your image or Yocto?
Did you manually build the QT?
Also can you mail me your configuration script? There could be a possibility that the QT is not properly built.
Regards,
nishad
Hi Nishad,
Thanks for replying.
I am using LTIB for building my image.
yes, I built QT4.8 manually with steps as mentioned on this page.
Also, the configuration script is same as given here.
./configure -qpa -arch arm -xplatform qws/linux-imx6-g++ -no-largefile -no-accessibility \
-opensource -verbose -system-libpng -system-libjpeg -system-freetype -fast -opengl es2 -egl -confirm-license \
-qt-zlib -qt-libpng -no-webkit -no-multimedia \
-make examples -make demos \
-release -make libs -exceptions -no-qt3support -prefix /opt/qt4.
Regards,
Paritosh Singh
These patches are for Qt4 not for Qt5 right?
Hi all PrabhuSundararaj
The git url "git://gitorious.org/qt/qt5.git qt5" is not work.
Is it new git url for qt5 ? Because I want to use LTIB porting Qt5.
Please help, thanks all.
Hello All,
is anyone able to compile QT5.5 or QT 5.6 for imx6q. This page is not helping me much because QT 5 compilation section referring the gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 fsl tool chain whcih is not available for download because it is pretty quite old.If i am using linaro latest tolchain 4.8 or 4.7 QT doesn't compile.
I would really appreciate if someone let me know which is the correct tool-chain to compile QT 5.5 or QT 5.6 version on imx6.
Hi nishad
I have successfully build Qt4.8.5 for imx6. But when I tried to run the sample example I got the below error:
root@freescale /opt/qt4.8.5-arm-opengl$ cd examples/opengl/hellogl_es2/
root@freescale /opt/qt4.8.5-arm-opengl/examples/opengl/hellogl_es2$ ls
bubble.cpp glwidget.h main.cpp texture.qrc
bubble.h hellogl_es2 mainwindow.cpp
glwidget.cpp hellogl_es2.pro mainwindow.h
<-opengl/examples/opengl/hellogl_es2$ ./hellogl_es2
bubble.cpp glwidget.h main.cpp texture.qrc
bubble.h hellogl_es2 mainwindow.cpp
glwidget.cpp hellogl_es2.pro mainwindow.h
<-opengl/examples/opengl/hellogl_es2$ ./hellogl_es2 -platform eglfs
Segmentation fault
root@freescale /opt/qt4.8.5-arm-opengl/examples/opengl/hellogl_es2$
Hi All
I have QT5.5.0, i want to crosscompile into imx6-linux. So i used the following configuration
./configure -v -opensource -confirm-license -no-pch -no-xcb -no-opengl -opengl es2 \
-make libs -device imx6 \
-compile-examples \
-device-option CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi- \
-sysroot /home/zumi/Project/Imx6q/rootfs/L3.0.35_4.1.0_130816_images_MX6/Rootfs/opt/qt -no-gcc-sysroot \
-prefix /opt/qt-vision
Following error i am getting,
cc1plus: error: unrecognized command line option '-fuse-ld=gold'
arm-fsl-linux-gnueabi-g++ -o libtest.so -shared -Wl,-Bsymbolic-functions -fPIC bsymbolic_functions.c
bsymbolic_functions.c:2:2: error: #error "Symbolic function binding on this architecture may be broken, disabling it (see QTBUG-36129)."
Symbolic function binding disabled.
And one more thing,
QT5.5.0 didn't have qws.conf file. so in your attached qmake.conf file i remove include(../../common/qws.conf) line.
If i not remove the line it shows No such a file found error. After the removing i got the above mentioned error.
Regards,
Aravinth
Hello every one,
How to configure and build Qt5.5 for INTEGRITY RTOS???
Hi bharathadwajakodanda,
In your Qt source Below location can you select which device you want to use:
~/qt5.5/qtbase/mkspecs/devices/
After that i will give you the support.
Hi aravinth,
Yeah, you got my point. There is no target device platform for INTEGRITY in
qt5.5/qtbase/mkspecs/devices/.
Is there any possibility to create target platform in
qt5.5/qtbase/mkspecs/devices/
by our own??
This is the full command I used to configure the target
configure -embedded -xplatform qws/integrity-arm-cxarm -prefix /
-qt-sql-sqlite
-embedded - builds the embedded version of Qt
-xplatform qws/integrity-arm-cxarm - selects the arm-cxarm mkspec for
INTEGRITY
-qt-sql-sqlite - links sqlite directly into the Qt library
According to my task the target should be integrity-arm-cxarm
On Fri, Aug 12, 2016 at 7:50 AM, aravinthkumar jayaprakasam <
I already done with it.
On Fri, Aug 12, 2016 at 10:43 AM, aravinthkumarjayaprakasam <