Boot The i.mx6 dual With Linux+uC/OS-II AMP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot The i.mx6 dual With Linux+uC/OS-II AMP

Boot The i.mx6 dual With Linux+uC/OS-II AMP

Author:Fourier Email:samssmarm@gmail.com

AMP:(Asymmetric Multiple Processing)

Scenario:cpu core 0 run Linux, cpu core 1 run uC/OS-II RTOS. HDMI display panel link to Linux, LCD display panel link to uC/OS-II RTOS.

Platform:

Mars Board(freesclae i.mx6 dual Coretex-A9 core, 1GB 64bit DDR3)

Panda Board(TIOMAP4460 dual Cortex-A9 core, 1GB 32bit DDR3)

Altera SoC EVMBoard(dual Cortex-A9 core, (512MB+256MB ECC) DDR3 on HPS, 512MB on FPGA)

Video Demo On Mars Board:

Youtube: http://youtu.be/yb6KC6Cf8i4

http://youtu.be/1uzrX-YZBnQ

Youku: http://v.youku.com/v_show/id_XNTMyNTAzNjky.html

AMP Port:

Linux SMP boot procedure is not mention here, For detail about the Linux SMP boot procedure please refer to the document here,http://www.linux-arm.org/LinuxBootLoader/SMPBoot.I just move the boot secondary procedure from Linux to U-boot as figure 1 in the AMP implementation, and figure2 describe the GIC relationship between two core and physical memory layout between Linux and uC/OS-II.

Figure 1

Figure 2

Display Subsystem Block on Mars Board and Panda Board:

Figure 3 imx6 display subsystem(Mars Board)

Figure 4 omap4460 display subsystem on panda board


コメント

hello,
thanks for illustration but how could i get the port for ucOS-II??
regards

can u list the source code for the porting layer or the illustration about it on cortex a9  thnx in advance

Hi,

I would thank you for this demonstration.

I am a beginner to IMX6 product and I want to use two different OS as you (one for HMI and the other one for computation/control).

Is there a memory latency due to each OS tries to access the memory at the same time?

If yes do you know the how long time are needed?

Thanks for your information

Hi,

Thanks a lot for your presentation.

i have the RTOS image in ELF format. May i know how to load and execute the same in secondary cores?

my entry point is 0x30000000. 

1. i have used "fatload mmc 1:1 0x30000000 rtos.elf" to load the image in U-boot console.

2. "cpu 1 release 0x30000000" but nothing works

could you please help me to solve this issue?

Thanks in advance

評価なし
バージョン履歴
最終更新日:
‎04-02-2013 11:45 PM
更新者: