qn9080sip "wireless uart""Read" " characteristic UUID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qn9080sip "wireless uart""Read" " characteristic UUID

686件の閲覧回数
1758793535
Contributor I

BCPT_$F_2S76$V%%PB`MD8D.pngD932FAA633C663528D348CF796F09DE4.jpgI can only see the " write characteristic UUID  " here, and only write operation can be performed. What should I do to read the data sent to me by the board with my mobile phone.

Thank you in advance

0 件の賞賛
返信
2 返答(返信)

654件の閲覧回数
nxf56274
NXP Employee
NXP Employee

If you can't download the apk, you can access http://d.firim.pro/fgx5 to download. This is a third-party website for test download.

0 件の賞賛
返信

675件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

nfr connect is used to learn the ble protocol. This test should used our app. You can download the app in this link 'https://play.google.com/store/apps/details?id=com.freescale.kinetisbletoolbox'

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信