qn9080sip "wireless uart""Read" " characteristic UUID

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qn9080sip "wireless uart""Read" " characteristic UUID

685 次查看
1758793535
Contributor I

BCPT_$F_2S76$V%%PB`MD8D.pngD932FAA633C663528D348CF796F09DE4.jpgI can only see the " write characteristic UUID  " here, and only write operation can be performed. What should I do to read the data sent to me by the board with my mobile phone.

Thank you in advance

0 项奖励
回复
2 回复数

653 次查看
nxf56274
NXP Employee
NXP Employee

If you can't download the apk, you can access http://d.firim.pro/fgx5 to download. This is a third-party website for test download.

0 项奖励
回复

674 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

nfr connect is used to learn the ble protocol. This test should used our app. You can download the app in this link 'https://play.google.com/store/apps/details?id=com.freescale.kinetisbletoolbox'

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复