pcie8997 wifi module Firmware Init Failed in imx8mmevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pcie8997 wifi module Firmware Init Failed in imx8mmevk

2,221 Views
js_wang
Contributor I

I had a problem about pcie8997 driver loading issue(Firmware Init Failed).
I had downloaded pcie8997 driver code form NXP web site
and we build pcie8997 driver by yocto cross compiler.
we put associated files to target imx8mmevk target borad.
Firmware Init Failed issue happend !

pcie8997 driver version :
      (1)PCIE-WLAN-UART-BT-8997-U16-X86-W16.68.10.p16-16.26.10.p16-C4X16640_V4-GPL
      (2)PCIE-WLAN-UART-BT-8997-U16-X86-W16.68.10.p16-16.26.10.p16-C4X16640_V4-MGPL

GPL and MGPL have the same result.

The load driver procedure as following
cp pcie8997_wlan_v4.bin /lib/firmware/mrvl/pcie8997_wlan_v4.bin
insmod mlan.ko
insmod pcie8xxx.ko drv_mode=1 fw_name=mrvl/pcie8997_wlan_v4.bin cfg80211_wext=0xf ps_mode=2 auto_ds=2
[ 7357.409516] wlan: Loading MWLAN driver
[ 7357.413978] rx_work=1 cpu_num=4
[ 7357.421952] Request firmware: mrvl/pcie8997_wlan_v4.bin
[ 7367.968345] FW failed to be active in time!
[ 7367.972553] WLAN: Fail download FW with nowwait: 0
[ 7367.977440] woal_request_fw failed
[ 7367.980865] Firmware Init Failed
[ 7367.986271] woal_pcie_probe: failed
[ 7367.989806] wlan_pcie: probe of 0000:01:00.0 failed with error -14
[ 7367.996090] wlan: Driver loaded successfully

would you help me to solve this problem 

   Thank you 

0 Kudos
Reply
1 Reply

2,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi J S

one can look at

mwifiex: PCIe8997 chip specific handling - Patchwork 

and try to debug if correct firmware loaded in driver code:

pcie.c\mwifiex\marvell\wireless\net\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply