kw41z zigbee home automation profile 1.2??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kw41z zigbee home automation profile 1.2??

737 Views
gustcool2
Contributor II

Hi 

I bought zha 1.2 sensor and want to connect sensor and kw41z board

Is it possible?

And can I use nxp zigbee home automation sdk?

I wonder if kw41z supports zigbee home automation profile 1.2.

thanks

1 Reply

697 Views
nxf63973
NXP Employee
NXP Employee

Hi JunTae Lee

 

The FRDM-KW41Z supports the standard IEEE 802.15.4, which is the base for the ZigBee Mesh Networking protocol.

 

It implements the ZigBee 3.0 device profile, including the configurations and support for the previous Home Automation profile. The Zigbee stack provided in the SDK implements the Zigbee 3.0 profile, so it should be compatible with your Home Automation device profile Sensor.

 

Please let me know if you need more information.