Hi NXP:
As jn5169 datasheet mention, the tx power can be set 10, 8.5 or 3 dbm
I'd want to ask how to set in the an1218 example?
Thanks a lot
Chris
Solved! Go to Solution.
HI mario:
Thanks for reply
And what is the default tx power for JN5169-001-M00-2 (my dev kit is JN516x-EK004)
Regards,
Chris
Hi Chris,
By default, the maximum power is enabled in our examples.
Regards,
Mario
Hi Mario:
Could you also tell me what is the default tx power of EH_switch of AN1219?
(Because from RF engineer test, the dimmable_light of AN1218 on JN5169-001-M00-2, is higher than EH_Switch around 4.)
Regards
Hi Chris,
It depends on the module that you are working on.
You could enable the high power
/* Define HIGH_POWER_ENABLE to enable high power module */
#ifdef HIGH_POWER_ENABLE
Regards,
Mario