jn5169 an1218 transmit power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

jn5169 an1218 transmit power

Jump to solution
876 Views
chriswei
Contributor II

Hi NXP:

As jn5169 datasheet mention, the tx power can be set 10, 8.5 or 3 dbm

I'd want to ask how to set in the an1218 example?

Thanks a lot

Chris

Labels (2)
0 Kudos
1 Solution
718 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chris,

Please see the files attached.

Regards,

Mario

View solution in original post

5 Replies
718 Views
chriswei
Contributor II

HI mario:

 

Thanks for reply

And what is the default tx power for JN5169-001-M00-2  (my dev kit is JN516x-EK004)

 

Regards,

Chris

0 Kudos
718 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chris,

By default, the maximum power is enabled in our examples.

Regards,

Mario

0 Kudos
718 Views
chriswei
Contributor II

Hi Mario:

Could you also tell me what is the default tx power of EH_switch of AN1219?

(Because from RF engineer test, the dimmable_light of AN1218 on JN5169-001-M00-2, is higher than EH_Switch around 4.)

Regards

0 Kudos
718 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chris,

It depends on the module that you are working on.

You could enable the high power

/* Define HIGH_POWER_ENABLE to enable high power module */
#ifdef HIGH_POWER_ENABLE

Regards,

Mario

0 Kudos
719 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Chris,

Please see the files attached.

Regards,

Mario