Hello,
According to JN-UG-3099, we can write MAC address, AES key and userdata in an OTP area of the JN5169.
3 x 128 bits words are reserved for user data. That is said, now how the application firmware can read these words?
Best regards
Benoit
yeah have been facing this issue since last couple of days....I hope i get an appropriate solution here myccpay
Hi,
These are attached in the zip and should be copied into the Componenets\HardwareAPI\Include Folder of your SDK.
Reads back the MAC address. Passing TRUE in bReadCustomerMACID causes the customer MAC address to be read, otherwise, the default MAC address is read.
PUBLIC bool_t bAHI_ReadMACID(
bool_t bReadCustomerMACID,
uint64 *pu64CustomerMACId);
Reads back the security key.
PUBLIC bool_t bAHI_ReadUserData(
uint8 u8UserFieldIndex,
uint32 au32userData[4]);
Reads back user data.
PUBLIC bool_t bAHI_ReadUserData(
uint8 u8UserFieldIndex,
uint32 au32userData[4]);
Hope it helps.
Regards,
Mario
Hi Mario,
Thank you, yes I think it will help me.
Best regards
<https://www.otodo.com/>
33 avenue du Maine
75015 Paris
www.otodo.com<http://www.otodo.com/>;
Benoit Roué
Lead Developer Embedded Software
benoit.roue@otodo.com<mailto:benoit.roue@otodo.com>
06.64.52.10.20
<https://www.facebook.com/OtodoOfficiel/>[Twitter icon]<https://twitter.com/OtodoOfficiel>[Linkedin icon]<https://www.linkedin.com/company/otodo/?lipi=urn%3Ali%3Apage%3Ad_flagship3_company_admin%3BJ1FpXoKeRwWGYatbYhzdaQ%3D%3D>[Youtube icon]<https://www.youtube.com/channel/UCHC7TXW-IldDkKhoZ8MAfMA?view_as=subscriber>
De : mario_castaneda <admin@community.nxp.com>
Envoyé : mardi 28 mai 2019 22:20
À : benoit roue <benoit.roue@otodo.com>
Objet : Re: - Re: how to read JN5169 userdata?
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: how to read JN5169 userdata?
reply from Mario Ignacio Castaneda Lopez<https://community.nxp.com/people/mario_castaneda?et=watches.email.thread> in Wireless Connectivity - View the full discussion<https://community.nxp.com/message/1157392?commentID=1157392&et=watches.email.thread#comment-1157392>
Hi Benoit,
Please look at the next community post.
https://community.nxp.com/thread/488670
Regards,
Mario
Hi Mario,
Thank you for your fast reply. In the mentioned community post, they only talk about the MAC address.
However, my question is about the 3 words of userdata, here is how to write it in the chip:
Once these date are written, how read them from the application firmware?
Best regards
<https://www.otodo.com/>
33 avenue du Maine
75015 Paris
www.otodo.com<http://www.otodo.com/>;
Benoit Roué
Lead Developer Embedded Software
benoit.roue@otodo.com<mailto:benoit.roue@otodo.com>
06.64.52.10.20
<https://www.facebook.com/OtodoOfficiel/>[Twitter icon]<https://twitter.com/OtodoOfficiel>[Linkedin icon]<https://www.linkedin.com/company/otodo/?lipi=urn%3Ali%3Apage%3Ad_flagship3_company_admin%3BJ1FpXoKeRwWGYatbYhzdaQ%3D%3D>[Youtube icon]<https://www.youtube.com/channel/UCHC7TXW-IldDkKhoZ8MAfMA?view_as=subscriber>
De : mario_castaneda <admin@community.nxp.com>
Envoyé : vendredi 17 mai 2019 02:16
À : benoit roue <benoit.roue@otodo.com>
Objet : Re: - Re: how to read JN5169 userdata?
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: how to read JN5169 userdata?
reply from Mario Ignacio Castaneda Lopez<https://community.nxp.com/people/mario_castaneda?et=watches.email.thread> in Wireless Connectivity - View the full discussion<https://community.nxp.com/message/1152774?commentID=1152774&et=watches.email.thread#comment-1152774>
Hi Benoit,
File zps_apl_aib.h
typedef struct
{
uint32 u32OutgoingFrameCounter;
uint16 u16ExtAddrLkup;
uint8 au8LinkKey[ZPS_SEC_KEY_LENGTH];
} ZPS_tsAplApsKeyDescriptorEntry;
ZPS_psGetActiveKey
Regards,
Mario
Hi Mario,
Since this function is doing a search by using a IEEE address, it doesn't tell me how to use it for reading raw data from the userdata.
Is there a particular way to write the userdata first?
Best regards
Hi Benoit,
You can find your own address in the next struct MAC_ExtAddr_s; mac_sap_CombineMac.h.
Please look at the https://www.nxp.com/docs/en/user-guide/JN-RM-2013.pdf
typedef tuAES_Block AESSW_Block_u;
Regards,
Mario