I was curious about creating a zigbee packet sniffer using the FRDM-KW41Z devkit and Wireshark.
Is there an easy way to do this?
Do I require the USB dongle to be able to sniff zigbee packets?
Hi apnagy@silabs.com,
Please see some details in the following topic USB-KW41 BLE Sniffer Application Update
Let us know if you need more details,
Regards,
Ovidiu
Thanks for the reply Ovidiu,
I've tried that guide and experienced the following:
FRDM-KW41Z plugged into a USB port.
I've flashed the mentioned firmware "KW41_802.15.4_SnifferOnUSB.bin" to the device.
After which the device LED4 lights up.
At this point I've tried the Protocol Analyzer Adapter and the Protocol Analyzer panel in the NXP Test Tool.
But neither can detect my connected KW41Z.
Is there an other firmware I need to flash for the FRDM-KW41Z?
Regards,
Árpád