I am following "JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool" as an initial basis for my application. I have the following includes:
#include <AppHardwareApi.h>
#include <JPT.h>
When I try to compile and link the following command:
mac = ZPS_u64AplZdoGetIeeeAddr(); //Get device MAC address
I get the following linker messages for the resulting error:
C:\Users\RRICHA~1\AppData\Local\Temp\ccKiZs35.ltrans1.ltrans.o: In function `AppColdStart':
ccKiZs35.ltrans1.o:(.text+0x104): undefined reference to `ZPS_u64AplZdoGetIeeeAddr'
ccKiZs35.ltrans1.o:(.text+0x104): relocation truncated to fit: R_BA_18_PCREL against undefined symbol `ZPS_u64AplZdoGetIeeeAddr'
collect2.exe: error: ld returned 1 exit status
make: *** [AN1172_CustomerModuleEvalTool_JN5169.elf] Error 1
What am I missing in the setup to be able to access this function?
RESOLVED ISSUE: I found the resolution for this problem. It is very simple, but hard to find. With my current setup, the 64-bit MAC address for the NXP JN5169 IC is read directly as follows: "mac = u64JPT_MacAddress;". Hope this helps someone else having the same issue. Thanks to those who offered suggestions along the way. Note that the "ZPS_u64AplZdoGetIeeeAddr();" function is not used in this development environment.
Estephania,
I had already found the link you sent me to. It tells how to code the ZPS_u64AplZdoGetIeeeAddr instruction into my application, but it does not tell me how to set up BeyondStudio and which #include files are needed to access the ZPS_u64AplZdoGetIeeeAddr instruction. The issue I have is that the linker is not finding the instruction. If you can help me to get the development environment to find the instruction I would be most appreciative.
1) I need to know what SKD is needed to access the ZPS_u64AplZdoGetIeeeAddr instruction
2) I need to know if #include files are needed to reference external files.
Thanks,
Randy
Hi Randy,
The ZPS_u64AplZdoGetIeeeAddr is part of the Zigbee Stack, it that the reason why you are getting the error message.
You are working on the JN-AN-1172 example, the SDK that it needs is the JN-SW-4163 IEEE 802.15.4.
I recommend looking at the MAC_ExtAddr_s, mac_sap_MiniMac.h
/**
* @brief Structure for MLME-ASSOCIATE.response
*
* Association response. Use type MAC_MLME_RSP_ASSOCIATE
*/
typedef struct
{
MAC_ExtAddr_s sDeviceAddr; /**< Device's extended address */
uint16 u16AssocShortAddr; /**< Short address allocated to Device */
uint8 u8Status; /**< Status of association */
uint8 u8SecurityEnable; /**< True if security is to be used on command frames 2003*/
MAC_SecurityData_s sSecurityData; /**< 2006 security*/
} MAC_MlmeRspAssociate_s;
Hope it helps.
Regards,
Mario
Mario,
I entered the structure you sent below. My development system did not locate 'MAC_ExtAddr_s' or 'MAC_SecurityData_s'. The following compiler error messages occurred:
c:/NXP/bstudio_nxp/workspace/JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool/AN1172_CustomerModuleEvalTool/Source/AN1172_CustomerModuleEvalTool.c:150:3: error: unknown type name 'MAC_ExtAddr_s'
c:/NXP/bstudio_nxp/workspace/JN-AN-1172-JN516x-Customer-Module-Evaluation-Tool/AN1172_CustomerModuleEvalTool/Source/AN1172_CustomerModuleEvalTool.c:154:6: error: unknown type name 'MAC_SecurityData_s'
Do I need to have some #include statements to help the compiler locate these types?
I also do not know how to call this structure to get the actual MAC address in my code. I would need to make some sort of call to get data into the structured variable. Can you give an example of how this is done?
Thanks,
Randy Richardson, P.E.
DPI-IPG Division Manager
801-747-0723 (office) 801-824-7736 (mobile)
250 West Berger Lane, Salt Lake City UT 84107
877-838-0534 801-270-2140 Fax: 801-281-2880
www.drillingproductsinc.com<http://www.drillingproductsinc.com/>;