Sudden change in volume of the BT speaker after bluetooth reconnection to DUT.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sudden change in volume of the BT speaker after bluetooth reconnection to DUT.

812 Views
virti_choksi
Contributor III
I am currently working with an 88W8997 chipset, and here are the details of my DUT setup:
 
Wi-Fi Driver: SD-WLAN-SD-BT-8997-U16-MMC-W16.68.118.p1-16.26.118.p1-C4X16693_V4-MGPL
Processor: BG5CT
OS: Android 12
Linux version: 4.9.178
 
Goal:
Check the volume of the BT speaker after reconnection to DUT.
 
Different scenarios to check the volume stability of BT speaker:
    I. BT adapter off/on 
       Use the command: svc bluetooth disable and
                                        svc bluetooth enable
 
    II. BT speaker/headset power off/on
              Manual power off
              Manual power on
 
test steps:
1. Connect the BT speaker with the DUT.
2. play YouTube video.
3. Disconnect the BT speaker by turning OFF the BT adapter or BT speaker.
4. Reconnect the BT speaker to DUT by turning ON the BT adapter or BT speaker.
5. repeat the test steps 50 times and more.
 
observation: Sometimes we observed a change in volume after reconnection of the BT speaker to DUT.

Best Regards,
Virti Choksi
0 Kudos
Reply
13 Replies

741 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

What is the issue frequency?

Can you please help to provide logcat logs, BT snoop logs and OTA sniffer logs(if possible)? 

I think it is better to check logs and reproduce this issue might be difficult on my side because you are using old Linux kernel version with Android 12.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

722 Views
virti_choksi
Contributor III

Hello @Christine_Li,

What is the issue frequency?

>> I performed the test for 50 iterations with some delay, and the issue frequency is 70 to 80 percent.

I have attached the requested logs below.

NOTE: This log file only contains one iteration when the volume suddenly increased, not 50 iterations.

Best regards,

Virti Choksi

0 Kudos
Reply

715 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi @virti_choksi 

Thanks for providing me logs.

From the given logs, I saw the AVRCP volume changed command is sent from Android host side.

Our BT chip is only just follow this command and sent it to remote BT side.

So please help to check on your host side.

I suggest you to compare the failed logs and success logs to find why host send this command.

I doubt it might be related to Absolute Volume feature. 

 

Best regards,

Christine.

 

Tags (1)
0 Kudos
Reply

711 Views
virti_choksi
Contributor III

Hello @Christine_Li,

I'm attaching the log below for one iteration when we got the previously set volume after reconnection.

Best regards,

Virti Choksi

0 Kudos
Reply

689 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

Can you please help to try after disabled the Absolute Volume on your host Android platform?

Usually, it is in Settings->Developer Options->Disable absolute volume.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

679 Views
virti_choksi
Contributor III

Hello @Christine_Li,

I've checked the Settings on our Android device but couldn't locate the option to disable Absolute Volume in the Developer Options section. It seems that this setting might not be available on our device or under a different menu.

Could you please confirm if there's an alternative method to disable Absolute Volume, or if there are any specific instructions we should follow?

Best regards,

Virti Choksi

0 Kudos
Reply

667 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

Can you see "Developer Options" in Settings?

If you can not see "Developer Options"  in settings, you need to click "About phone" Or "About Tablet" or something like this. Then click 7 times on the Build Number menu, it will show a toast to remind you that you are now a developer.

Then go back to Settings ->System-> you can see Develop options.

Then you can directly search "Absolute" word to see where is "Absolute volume" option located.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

663 Views
virti_choksi
Contributor III

Hello @Christine_Li,

Can you see "Developer Options" in Settings?
>> Yes, the Developer option is enabled.

However, I still could not find the absolute volume disable option.

Best regards

Virti Choksi

0 Kudos
Reply

658 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

How about search the key word "Absolute" ?

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

565 Views
virti_choksi
Contributor III

Hello @Christine_Li,

Could you please confirm if there's an alternative method to disable Absolute Volume?

Best regards,

Virti Choksi

0 Kudos
Reply

560 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

Sorry, I am not familiar with your host platform, I don't whether have other alternatives to disable absolute volumes.

And also please see my previous analysis, it should be host side issue. Our BT controller receive this volume change command from host, then send it to remote side. So the root cause is from host side, not our controller side.

 

Best regards,

Christine.

0 Kudos
Reply

642 Views
virti_choksi
Contributor III

Hi @Christine_Li,

In our device we do not have search option in settings.

Best regards,

Virti Choksi

0 Kudos
Reply

770 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @virti_choksi 

Thanks for creating case to us.

I will deal with this case and try to reproduce on my side, once have any updates, I will share with you.

 

Best regards,

Christine.

0 Kudos
Reply