I have OM15080-K32W dongle and try to run Kinetis Protocol Analyzer with Wireshark, it only works in 802.15.4 but BLE. From KPAA, it seems the BLE filter is disabled and cannot be checked(as below screenshot).
Please advise how to use OM15080-K32W as BLE sniffer?
Need to reflash firmware? If yes, where can I get this firmware?
Thanks a lot!
Herman
Solved! Go to Solution.
Hi @HermanLin,
I hope you are doing great.
We do not provide any bin file for the QN9090 to be configured as Bluetooth LE Sniffer. Sorry for any inconvenience that this may cause you.
However, the MCU that could capture these packets over the air is the USB-KW41/KW36/KW38.
Bluetooth LE Sniffer Application Update
Regards,
Mario
Hi Mario,
Thanks for your great support!
Best Regards,
Herman