I have a QN9080 chip customized board.
I want to debug this chip board using JTAG interface on QN908x Development board.
Is there any document explaining the steps required for this or the setup?
I have tried the following but it is not working, can someone point out what I am doing wrong?
The setup is as follows:
1. Short Jumper JP1 on NXP QN908x Development board.
2. Take JTAG 10-pin connector and connect it to the custom board as follows:
- Connect Vcc , GND, SWDIO, SWDCLK, SWO and Reset pin.
- I have kept ISP_Detect, IF_Detect and JTAG_TDI pins open as it is not connected to the QN908x chip.
Is this setup correct or I missed something?
Attached is the 10-pin Debugger connector pinout.
Can someone please help me with this, its Urgent.
解決済! 解決策の投稿を見る。
Dear Ankur,
If you check in the DK User’s Guide the chapter "3.1.2 CMSIS-DAP to off-board target" you can check the jumper configuration to degub you custom board .
I hope this helps you.
Best Regards,
Alexis Andalon
Dear Ankur,
The QN908x doesn’t support the JTAG protocol for debugging, only SWD.
Best Regards,
Alexis Andalon
Thanks Alexis for the response.
So, I was using JTAG 10-pin Connector which also has SWD lines.
So, here what exactly I am trying to do is, I want to Debug my Customized QN908x board.
It has SWD as well as JTAG pin exposed.
While going through the "QN908x-DK-User Guide", I have read that "P1" can be used to debug the external QN908x chip.
I want to know what exact setup needed to debug the chip.
I have tried this using two QN908x Development board V1.2 and I am able to Debug using "P1" Connector. But, the same thing I want to do on our QN908x Customized Dev Board.
Dear Ankur,
If you check in the DK User’s Guide the chapter "3.1.2 CMSIS-DAP to off-board target" you can check the jumper configuration to degub you custom board .
I hope this helps you.
Best Regards,
Alexis Andalon
Thanks a lot Alexis,
It is working now. I was powering up the Board using Development board.
Changing jumper setting on JP2 makes it work.