Dear Sir
I can’t see NXP_OTAA in IOT Tool box after I follow API Guide based on newest QN9080 SDK.
Could you try it in your side and make sure if NXP_OTAA can show in the app?
BR
Lee Wang
Hello,
Just to make sure I fully understand you.
You used the OTA, flashed a new firmware, and you can't perform the OTA again? If you flashed a new firmware, I believe that was an example, do you see the example functionality in the application?
I mean, if you loaded a heart rate sensor, do you see it in the app?
Regards,
Estephania
hello, i test otap in qn9080 board,with client att code, after programing first time when i update using otap ,code uplode and work properly. but second time it not update it restart from 1% again and again
You said "second time it not update it restart from 1% again and again". Could you make sure if you still see OTAP_Client_ATT after you performed 1st OTAP ? I think it already been flashed update by your application.
You need to integrate OPTA_Client_ATT with your application first, then perform OTAP. After that, you may can perform 2nd OTAP process.
Hi Jason,
I'm in a process of developing a multiple otap capability application, Due to memory constraints it seems difficult for 3 image spaces in the flash memory. would you please ellaborate the sentence "integrate OPTA_Client_ATT with your application first". I just stuck in there ..lol
Thanks in Advance :smileyhappy:
Simple to say : we haven't default code for the requirement of " performing 2nd OTAP ". What profile you used in your application ? You need to integrate OTAP_ATT_Client project file into your profile code for your application running 2nd OTAP. Hoping this explain it.
Hi Jason. Actually I figured out it without integrating the otap profile. Thanks for the Help :smileyhappy:
Would you please share your idea ?
Sure Jason. I'm preparing a blog post. I'll update the link to the page once i finished. :smileyhappy:
Thanks Jason. I'm working on it.:)
i have the similar issue,In mine it is showing OTAL while sending the file,after that it will show transfer completed,and that code functionality is not visible .Can u guide me #estephania
which file u sending?,because in any code u need to creat otap service for example otap server or otap client code