Good day,
We are developing a project using the PN5180 in card emulation mode. The device is going into an Autocoll mode and the interrupt is working well. If I read the IRQ_STATUS register value I get 0x00000011 which means that IRQ_STATUS_RX_IRQ_MASK and IRQ_STATUS_CARD_ACTIVATED_IRQ_MASK are ON. The problem is when I try to read RX_STATUS register, to know how many bytes are in the buffer, I get 0x00. If I try to read the RX buffer anyway it returns me 0xC080.
Is it something wrong with the initial configuration? Can you please help me to resolve this?
Thank you
Solved! Go to Solution.
Hi @a_ivanov ,
We provide a card emulation demo in the project of "NfcrdlibEx8_HCE_T4T", you may fetch it from the latest NFC reader library for PN5180, for more details regarding receiving data, please kindly refer to phhalHw_Pn5180_Receive_Int() .
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @a_ivanov ,
We provide a card emulation demo in the project of "NfcrdlibEx8_HCE_T4T", you may fetch it from the latest NFC reader library for PN5180, for more details regarding receiving data, please kindly refer to phhalHw_Pn5180_Receive_Int() .
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------