MKW30Z rebuild Bootloader OTAP for new PCB layout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW30Z rebuild Bootloader OTAP for new PCB layout

835 次查看
lucianfiran
Contributor V

KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0); IAR 7.50

framework\Bootloader\Bootloader_OTAP_Serial

What hardware changes on new PCB will trigger a rebuild on the Bootloader_OTAP_Serial ?

If NO RTC 32KHz external quartz oscillator on new PCB then the boot loader code must be changed ?

Thank you,

Lucian

标记 (4)
0 项奖励
回复
2 回复数

644 次查看
lucianfiran
Contributor V

Project location framework\Bootloader

pastedImage_1.png

Target selection in project

pastedImage_2.png

or

pastedImage_3.png

Some parameters:

MCU_MKW40Z160
gEepromType_d=gEepromDevice_AT45DB021E_c

pastedImage_4.png

so gEepromType_d change should trigger a rebuild.

/* List of the EEPROM devices used on each of the FSL development boards */

gEepromDevice_None_c          0
gEepromDevice_InternalFlash_c 1
gEepromDevice_AT45DB161E_c    2 /* TWR-KW2x */
gEepromDevice_AT26DF081A_c    3 /* TWR-MEM */
gEepromDevice_AT45DB021E_c    4 /* TWR-KW4x*/

What about MCU change type from MCU_MKW40Z160 to MKW30Z  ?

Linker gRomSize_c=0x28000 param

pastedImage_9.png

other parameters might be:

gEepromParams_WriteAlignment_c, gEepromWriteEnable_d, gSerialBootloaderEnable_c,
gSPI_HW_TYPE_c, gSerialBootloaderEnable_c, BOOTLOADER_CRC_ENABLE, BOOTLOADER_ENABLE_VERIFY,
BOOTLOADER_ENABLE_READ_CMD, BOOTLOADER_INT_WATCHDOG  

What other HW PCB changes may trigger boot-loader re-builds ?

What about NO RTC 32KHz external quartz oscillator on new PCB ?

Thank you,

Lucian

0 项奖励
回复

644 次查看
carlos_neri
NXP Employee
NXP Employee

32KHz XTAL is not a requirement for the bootloader, so, you're safe on that end. But, you'll loose some low power capabilities.

Here're some scenarios the will requiere a bootloader re-build:

- Any change in the bootloader configuration

- Use different IC

- Use a different SPI module

- Use different pins

- Use different memory

- Add extra functionality 

0 项奖励
回复