Hello
My question is regarding the MKW24D512. When not using the VREGIN and VOUT33, what should be done with these pins? Can they be floating? Also when externally suppliyng the device instead of using internal regulator, are there any possible design changes?
Regards,
Mete
已解决! 转到解答。
Hello Mete,
If VREGIN and VOUT33 are not used it is recommended to let these pins floating. If your design uses external power supply there are no extra design changes required, but still you will have to preserve the bypass capacitors.
Best Regards,
Mihai Dragnea - Connectivity System Engineer
Hallo Mihai,
MKW24D512 Datasheet says that Supply voltage can vary b/w 1.8V-3.6V.
Is this MKW24D512 can be externally powered by a two series AAA batteries (voltage varies b/w 1.6V-3.2V)?
Thanks.
BR
Zeshan
Hello Mete,
Just checked again with my colleagues and I do have a different recommendation: you should tie VREGIN and VOUT33 together and to GND through a 10K resistor. Below you may find a table to serve you as an example:
Kind Regards,
Mihai
Hello Mete,
If VREGIN and VOUT33 are not used it is recommended to let these pins floating. If your design uses external power supply there are no extra design changes required, but still you will have to preserve the bypass capacitors.
Best Regards,
Mihai Dragnea - Connectivity System Engineer