Hello
My question is regarding the MKW24D512. When not using the VREGIN and VOUT33, what should be done with these pins? Can they be floating? Also when externally suppliyng the device instead of using internal regulator, are there any possible design changes?
Regards,
Mete
解決済! 解決策の投稿を見る。
Hello Mete,
If VREGIN and VOUT33 are not used it is recommended to let these pins floating. If your design uses external power supply there are no extra design changes required, but still you will have to preserve the bypass capacitors.
Best Regards,
Mihai Dragnea - Connectivity System Engineer
Hallo Mihai,
MKW24D512 Datasheet says that Supply voltage can vary b/w 1.8V-3.6V.
Is this MKW24D512 can be externally powered by a two series AAA batteries (voltage varies b/w 1.6V-3.2V)?
Thanks.
BR
Zeshan
Hello Mete,
It's from a different part but very similar to KW24. You should consider only the information related to VREGIN and VOUT33.
Regards,
Mihai
Allright, I'll consider this. Thanks Mihai.
Regards,
Mete
Hello Mete,
Just checked again with my colleagues and I do have a different recommendation: you should tie VREGIN and VOUT33 together and to GND through a 10K resistor. Below you may find a table to serve you as an example:
Kind Regards,
Mihai
Though I cant seem to find which pin corresponds to USB0_VSS? Can you point out to where that information is from?
Awesome, thanks for the feedback. I'll do as you have recommended.
Regards,
Mete
Hello Mete,
If VREGIN and VOUT33 are not used it is recommended to let these pins floating. If your design uses external power supply there are no extra design changes required, but still you will have to preserve the bypass capacitors.
Best Regards,
Mihai Dragnea - Connectivity System Engineer