[MKW01Z128] Radio operation with 32.768kHz xtal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MKW01Z128] Radio operation with 32.768kHz xtal

933 Views
giancarlozanuz
Contributor III

Hello, I'm facing some problems with the radio communication when using an external 32.768kHz crystal.

I'm using two KW01-MBR development boards and the examples from Connectivity Software. When I connect J8 (XTAL_32K jumper) to position 1 - 2 (PTA18 and DIO5/CLKOUT) and define in 'board.h' file CLOCK_INIT_CONFIG CLOCK_RUN, the program runs fine, I can send and receive messages with no problem.

But when I change to the external crystal in J8 to position 2 - 3 (PTA18 and EXTAL_32K_EXT), and define CLOCK_INIT_CONFIG CLOCK_XTAL, the program does not work well, and the radio interface does not work anymore.

Do I need to setup any other option or configuration to work with the external crystal? Thanks!

2 Replies

714 Views
luisburgos
NXP Employee
NXP Employee

Hi Giancarlo,

You also need to change the pin multiplexing in pin_mux.c for PTA18 and PTA19.

PTA18 and PTA19 are configured as MUX1 by default, but those pins need to be configured as MUX0, as shown in reference manual:

MUXS.png

For PTA18:

PTA18.png

PTA19:

PTA19.png

Best regards,

Luis Burgos.

714 Views
giancarlozanuz
Contributor III

It worked, thanks!