KW45 SPSDK burns NBU and locks up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 SPSDK burns NBU and locks up

Jump to solution
2,633 Views
Melton
Contributor III

Dear Sir,

  I encountered a problem that the chip locked after burning NBU through SPSDK.

1. chip type: KW45B41Z83A.

2. I downloaded the latest AN13883SW from the official website.

3. I followed this link to run SPSDK, then also successfully burned key and SB3 files.

KW45xx and K32W1xx Load NBU image — SPSDK documentation

Melton_1-1716455958496.pngMelton_2-1716456000892.png

4. Finally I burned the KW45 wireless uart routine,However, it does not work, and other mcu-related routines can run normally,similar to hello world routines, my board works fine.(SDK version:V2.12.5)

5.  Then I tried to update the SB3 file generated by SPSDK to the SB3 file within the SDK(version 2.12.5) via blhost,but they refused to burn it,errors in the following picture.

Melton_3-1716456622397.png

6. I can only burn the SB3 file generated by SPSDK through BLHOST, as shown below, but this SB3 file can not run the radio frequency routine.

Melton_4-1716456950812.png

 

So I would like to ask you what causes this,looking forward to your reply,thank you!

KW45 

0 Kudos
Reply
1 Solution
1,834 Views
nxa17177
NXP Employee
NXP Employee

Hello @Melton 

you can try to get the NBU image from SDK, which you would like to use and then change only a xip image and call the receive-sb-file again with newly generated sb file. Let me know if you still have a problem. 

View solution in original post

0 Kudos
Reply
22 Replies
943 Views
Boured
Contributor I

 I tried to burn NBU through SPSDK by looking at AN13883, The version of python I use is V3.11.6。But I had a problem running script 5.2.

0 Kudos
Reply
187 Views
nxa17177
NXP Employee
NXP Employee

@Boured could you please describe details of your problems? Could you share your workspace with me?

0 Kudos
Reply