K32W CTUG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W CTUG

1,580 Views
danieltseng
Contributor V

Refer to K32WQN9090CTUG.pdf

pastedImage_1.png

In RX test mode
[ 1 ]  RX trigger mode test  pastedImage_1.png
    What signal generator is used?
    No DIO17 pins on the circuit?
    When do I need to do this test?

[ 2 ]  RX continuous mode test

      When do I need to do this test?

Labels (1)
  • KW

0 Kudos
Reply
6 Replies

1,428 Views
Xiang_Li
NXP Employee
NXP Employee

>> [ 1 ]  RX trigger mode test
>>     When do I need to do this test?
>> [ 2 ]  RX continuous mode test
>>    When do I need to do this test?

Short answer:

If PER measurement required, use trigger mode. Else use continuous mode.

Trigger mode needs a trigger signal from the tester. Continuous mode doesn't.

Long answer:

For Rx continuous mode test, the DUT (device-under-test, aka, your design) just keeps receiving all packets, sent from a reference tester. At the end, software counts how many good packets are received (CRC check ok).

If any packet lost in the air, because of the RF interference or other reasons, in the Rx continuous test we will not know. Because we don't know how many packet in total should be received.

So we need the Rx trigger mode test. When the reference tester sends a packet, it also gives a pulse on a wire. This wire would be connected to the Rx side. By counting how many pulses on the wire, the Rx would know how many packet in total. And then it can calculated how many actual packet it received, as well as the PER (packet error rate).

>> What signal generator is used?

Check the RF tester being used. It probably has a trigger signal output, that will connect to your IUT device.


>> No DIO17 pins on the circuit?

I am not sure on this. I suggest you to check the SW implementation of the Certi tool on K32W and QN9090/30

1,428 Views
danieltseng
Contributor V

I have two questions, I will open another topic to ask.

K32W AN12798 bug1 

https://community.nxp.com/message/1342031 

0 Kudos
Reply

1,428 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Please check the posts and the internal answers as well.

Regards,

Estephania

0 Kudos
Reply

1,428 Views
danieltseng
Contributor V

I found two bug.
一。Ch2.3.2.3 of AN12798 requires unmodulate signal, but K32W_Certi_Tools does not have this option.

pastedImage_1.png

pastedImage_3.png

二。Frequency measurement also requires unmodulated continuous signal to be correct

pastedImage_2.png

 

0 Kudos
Reply

1,428 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello.

Could you please check the CW mode? it seems that you are referring to the modulated options.

pastedImage_16.png

Please refer to the JN-AN-1242-Customer-Module-Eval-Tool

Regards, 

Estephania

0 Kudos
Reply

1,428 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

I believe that to help you clarify the usage of the tool and the connections you are asking for, could you please help me check this application note?

Regards,

Estephania

0 Kudos
Reply