K32W AN12798 bug1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W AN12798 bug1

1,393 Views
danieltseng
Contributor V

< BLE test  on ch2 >

一。Ch2.3.2.3 of AN12798 requires unmodulate signal, but K32W_Certi_Tools does not have this option.

 

pastedImage_3.png

pastedImage_3.png

As follows, kw41 has provided it

pastedImage_2.png


Labels (1)
  • KW

0 Kudos
Reply
2 Replies

1,297 Views
Xiang_Li
NXP Employee
NXP Employee

I also don't understand why test in ch 2.3.2.3 asks for "unmodulated" signal, because for RF power test this shouldn't matter. And maybe it is even better to use modulated signal because it is more closed to reality use cases.

In fact in BLE RF test spec, RF-PHY/TRM/BV-01-C [Output power], it suggests to use PRBS9 payloads.

And if you look at this document Annex C, page 101, it says " [1], [5] or [6], then[q] or [w] ".

I think the AN12798 document owner should double check on this.

1,297 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

I believe there is a confusion , could you please let me know what you are trying to do and why are you using this demo ? Are you performing some tests for the certification of the product? Are you trying to make a certification or radio tests for Bluetooth LE or 802.15.14?

As mentioned previously in another thread, why are you using the Modulated TX tests and not the CW tests ?

Regards,

Estephania

0 Kudos
Reply