K32W AN12798 bug1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K32W AN12798 bug1

1,377 次查看
danieltseng
Contributor V

< BLE test  on ch2 >

一。Ch2.3.2.3 of AN12798 requires unmodulate signal, but K32W_Certi_Tools does not have this option.

 

pastedImage_3.png

pastedImage_3.png

As follows, kw41 has provided it

pastedImage_2.png


标签 (1)
  • KW

0 项奖励
回复
2 回复数

1,281 次查看
Xiang_Li
NXP Employee
NXP Employee

I also don't understand why test in ch 2.3.2.3 asks for "unmodulated" signal, because for RF power test this shouldn't matter. And maybe it is even better to use modulated signal because it is more closed to reality use cases.

In fact in BLE RF test spec, RF-PHY/TRM/BV-01-C [Output power], it suggests to use PRBS9 payloads.

And if you look at this document Annex C, page 101, it says " [1], [5] or [6], then[q] or [w] ".

I think the AN12798 document owner should double check on this.

1,281 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

I believe there is a confusion , could you please let me know what you are trying to do and why are you using this demo ? Are you performing some tests for the certification of the product? Are you trying to make a certification or radio tests for Bluetooth LE or 802.15.14?

As mentioned previously in another thread, why are you using the Modulated TX tests and not the CW tests ?

Regards,

Estephania

0 项奖励
回复