IW416 long time throughput performance down, disable enable_tcp_ack_enh to improve

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IW416 long time throughput performance down, disable enable_tcp_ack_enh to improve

873件の閲覧回数
yao_feng
Contributor III

Customer: Moxa

Platform: IMX6

OS: Linux

Customer found after long time throughput speed monitoring,
performance down as below:

uptime

bandwidth (Mbps)

5:21

26.7

5:44

23

12:32

15

13:19

12.4

 

Customer found after modify driver enable_tcp_ack_enh to force disable, can get improvement.

They wants to know
1. In Wifi driver, what's the purpose for enhance tcp ack?
2. any side effect if do disable enable_tcp_ack_enh?

Thanks.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

848件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Dear  @yao_feng ,

 

1. In Wifi driver, what's the purpose for enhance tcp ack?

tcp ack enhance will drop some TCP ACK packet and only transmit the last one.


2. any side effect if do disable enable_tcp_ack_enh?

No any effect. every tcp ack will be transmitted by wifi chip

 

So no problem to enable or disable it.

 

Regards,

weidong

0 件の賞賛
返信

840件の閲覧回数
yao_feng
Contributor III

Got it, thanks.

0 件の賞賛
返信

853件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

We will answer you internally 

0 件の賞賛
返信