IW416 long time throughput performance down, disable enable_tcp_ack_enh to improve

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IW416 long time throughput performance down, disable enable_tcp_ack_enh to improve

783 Views
yao_feng
Contributor III

Customer: Moxa

Platform: IMX6

OS: Linux

Customer found after long time throughput speed monitoring,
performance down as below:

uptime

bandwidth (Mbps)

5:21

26.7

5:44

23

12:32

15

13:19

12.4

 

Customer found after modify driver enable_tcp_ack_enh to force disable, can get improvement.

They wants to know
1. In Wifi driver, what's the purpose for enhance tcp ack?
2. any side effect if do disable enable_tcp_ack_enh?

Thanks.

Labels (2)
0 Kudos
Reply
3 Replies

758 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear  @yao_feng ,

 

1. In Wifi driver, what's the purpose for enhance tcp ack?

tcp ack enhance will drop some TCP ACK packet and only transmit the last one.


2. any side effect if do disable enable_tcp_ack_enh?

No any effect. every tcp ack will be transmitted by wifi chip

 

So no problem to enable or disable it.

 

Regards,

weidong

0 Kudos
Reply

750 Views
yao_feng
Contributor III

Got it, thanks.

0 Kudos
Reply

763 Views
vicentegomez
NXP TechSupport
NXP TechSupport

We will answer you internally 

0 Kudos
Reply