HW: IW416 Module (AW-AM457D) + .MX 6ULL
Platform: i.MX 6ULL
OS kernel version: Linux MOXA 4.4.0-cip-rt-moxa-imx6ull
WiFi driver/FW: 5.10.72/ sdiouartiw416_combo_v0.bin
Role: IW416 module be STA or UAP? STA
Reproduce steps: 客戶描述” 我們的的產品(iw416) 與 AP Cisco 91xx Series連接,然後idle 一段時間就會出現,但我們無法復現
Happen rate:
Log:
2024/06/28 09:31:33 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'
2024/06/28 09:31:33 freq=2412 rssi=-35 dBm
2024/06/28 09:31:33 02. 00:f6:63:79:59:c8 ssid='UKS-Klinik'
2024/06/28 09:31:33 freq=2437 rssi=-58 dBm
2024/06/28 09:31:33 03. 54:a2:74:57:cc:c8 ssid='UKS-Klinik'
2024/06/28 09:31:33 freq=2437 rssi=-64 dBm
2024/06/28 09:31:34 Connect to 00:df:1d:c4:4a:a1 on channel 1
2024/06/28 09:31:34 Authentication completed
2024/06/28 09:33:36 Disconnect from 00:df:1d:c4:4a:a1, reason=108
2024/06/28 09:33:38 Scan 12 APs, show the best 3 with the same SSID:
2024/06/28 09:33:38 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'
2024/06/28 09:33:38 freq=2412 rssi=-35 dBm
2024/06/28 09:33:38 02. 00:f6:63:79:59:c8 ssid='UKS-Klinik'
2024/06/28 09:33:38 freq=2437 rssi=-57 dBm
2024/06/28 09:33:38 03. 54:a2:74:57:cc:c8 ssid='UKS-Klinik'
2024/06/28 09:33:38 freq=2437 rssi=-65 dBm
2024/06/28 09:33:38 Connect to 00:f6:63:79:59:c8 on channel 6
2024/06/28 09:33:38 Authentication completed
2024/06/28 09:36:01 Disconnect from 00:f6:63:79:59:c8, reason=108
2024/06/28 09:36:03 Scan 11 APs, show the best 3 with the same SSID:
2024/06/28 09:36:03 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'
2024/06/28 09:36:03 freq=2412 rssi=-36 dBm
customer modified code(add print):
#ifdef MOXA_WLAN_LOG
{
char buf[120];
sprintf(buf, "MOXA_LOG=Disconnect from "FULL_MACSTR", reason=%d", FULL_MAC2STR(priv->cfg_bssid),reason_code);ç=我們只是把reason code印出來
woal_broadcast_event(priv, buf, strlen(buf));
}
#endif
@Christine_Li please help us to check reason code 108 meaning.
解決済! 解決策の投稿を見る。
Hi, @yao_feng
Thanks for creating case to us.
1. Customer is using too old driver and FW, it is recommended to use our latest driver and FW to have a try.
2. Whether this issue is only occurred in 2.4G? how about in 5G?
3.If possible, please request customer help to provide me Wi-Fi OTA sniffer logs to check what happened between STA and AP communication.
Best regards,
Christine.
Hi, @yao_feng
Thanks for creating case to us.
1. Customer is using too old driver and FW, it is recommended to use our latest driver and FW to have a try.
2. Whether this issue is only occurred in 2.4G? how about in 5G?
3.If possible, please request customer help to provide me Wi-Fi OTA sniffer logs to check what happened between STA and AP communication.
Best regards,
Christine.