IW416 - Deauthentication reason code 108 meaning?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IW416 - Deauthentication reason code 108 meaning?

Jump to solution
453 Views
yao_feng
Contributor III

HW: IW416 Module (AW-AM457D) + .MX 6ULL

Platform: i.MX 6ULL

OS kernel version: Linux MOXA 4.4.0-cip-rt-moxa-imx6ull

WiFi driver/FW: 5.10.72/ sdiouartiw416_combo_v0.bin

Role: IW416 module be STA or UAP? STA

Reproduce steps: 客戶描述” 我們的的產品(iw416) 與 AP Cisco 91xx Series連接,然後idle 一段時間就會出現,但我們無法復現

Happen rate: 

Log:

2024/06/28 09:31:33 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'                   
2024/06/28 09:31:33     freq=2412 rssi=-35 dBm                                
2024/06/28 09:31:33 02. 00:f6:63:79:59:c8 ssid='UKS-Klinik'                   
2024/06/28 09:31:33     freq=2437 rssi=-58 dBm                                
2024/06/28 09:31:33 03. 54:a2:74:57:cc:c8 ssid='UKS-Klinik'                   
2024/06/28 09:31:33     freq=2437 rssi=-64 dBm                                
2024/06/28 09:31:34 Connect to 00:df:1d:c4:4a:a1 on channel 1                 
2024/06/28 09:31:34 Authentication completed                                  
2024/06/28 09:33:36 Disconnect from 00:df:1d:c4:4a:a1, reason=108             
2024/06/28 09:33:38 Scan 12 APs, show the best 3 with the same SSID:          
2024/06/28 09:33:38 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'                   
2024/06/28 09:33:38     freq=2412 rssi=-35 dBm                                
2024/06/28 09:33:38 02. 00:f6:63:79:59:c8 ssid='UKS-Klinik'                   
2024/06/28 09:33:38     freq=2437 rssi=-57 dBm                                
2024/06/28 09:33:38 03. 54:a2:74:57:cc:c8 ssid='UKS-Klinik'                   
2024/06/28 09:33:38     freq=2437 rssi=-65 dBm                                
2024/06/28 09:33:38 Connect to 00:f6:63:79:59:c8 on channel 6                 
2024/06/28 09:33:38 Authentication completed                                  
2024/06/28 09:36:01 Disconnect from 00:f6:63:79:59:c8, reason=108             
2024/06/28 09:36:03 Scan 11 APs, show the best 3 with the same SSID:          
2024/06/28 09:36:03 01. 00:df:1d:c4:4a:a1 ssid='UKS-Klinik'                   
2024/06/28 09:36:03     freq=2412 rssi=-36 dBm

 

customer modified code(add print):

#ifdef MOXA_WLAN_LOG

{

           char buf[120];

           sprintf(buf, "MOXA_LOG=Disconnect from "FULL_MACSTR", reason=%d", FULL_MAC2STR(priv->cfg_bssid),reason_code);ç=我們只是把reason code印出來

           woal_broadcast_event(priv, buf, strlen(buf));

}

#endif

@Christine_Li  please help us to check reason code 108 meaning.

0 Kudos
Reply
1 Solution
413 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

Thanks for creating case to us.

1. Customer is using too old driver and FW, it is recommended to use our latest driver and FW to have a try.

2. Whether this issue is only occurred in 2.4G? how about in 5G?

3.If possible, please request customer help to provide me Wi-Fi OTA sniffer logs to check what happened between STA and AP communication.

 

Best regards,

Christine.

View solution in original post

Tags (1)
0 Kudos
Reply
3 Replies
432 Views
yao_feng
Contributor III
  • Wifi Firmware version:SDIW416---16.92.21.p11.2-MM5X16283.p2-GPL-(FP92)
  • Wifi mwifiex-linux-driver:V5.10.72_2.2.0
0 Kudos
Reply
414 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

Thanks for creating case to us.

1. Customer is using too old driver and FW, it is recommended to use our latest driver and FW to have a try.

2. Whether this issue is only occurred in 2.4G? how about in 5G?

3.If possible, please request customer help to provide me Wi-Fi OTA sniffer logs to check what happened between STA and AP communication.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply
354 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

Is there any updates from customer related on my request?

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply