Hi support team!
Relate to:
How to enable High Power on JenNet-IP w/ JN5168-001-M05/6?
Enabling High power on Jn5168-001-M05 | Zigbee 3.0
How to config JN5169 + SE2431 PA ?
Now I'm working with JN5169 module have SE2431 PA. As i know JN5169-001-M06-2 support hight Power and connect with SE2431 PA on pin 12,13
So. For enable Hight Power I have change something in JN-AN-1216 ControlBridge
=>> Build error:
Please help confirm
- Can you give advice for enable hight power?
- How to fix build error?
Thanks you so much!
Thank for your help!
Now I use Ubiqua for test Signal strength. Use 2 module NonPA and HavePA
JN5169 USB Dongle ubiqua capture RSSI seems like incorrect?
Maybe RSSI value is wrong! The value decreases with time.
Can you help me? :smileygrin:
Hi Tran,
The way that you are using is not the best way to measure dBm. However, it could give you an idea, but you could have a lot of variables and the RSSI could be stable.
By default, the JN devices have set the high power.
Regards,
Mario
Hi Tram & Mario,
Can you use it now? I use JN5169-001-M06-2, but the distance sent is only 5 meters.
I want to reach the maximum power and distance. Do you know how to do it?
How is this transmission power and distance calculated?
I have added to app_start.c
vAppApiSetComplianceLimits(0, -10, 81);
vAHI_HighPowerModuleEnable(TRUE, TRUE);
But I don't see anything change on Ubiqua
Can you make me clearly!
Hi Tram,
- Can you give advice to enable hight power?
Please look at the DR1191_JN5168_HP_uFL_M06_Module_1V0 folder, included in the JN-RD-6038 Lite. You could take as reference the schematic file.
- How to fix the build error?
Please add the next line in the makefile.
APPSRC += AHI_ModuleConfiguration.c
Regards,
Mario