Can KW2x support ZigBee 868 MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can KW2x support ZigBee 868 MHz?

1,568 次查看
benjaminchang
Contributor V

NXP KW2x is supporting 802.15.4, one of our customer is requesting ZigBee 2.4 GHz and 868 MHz (a GB requirement) since last year. So we proposed KW01Z + KW20Z to them. Checking the new EE Times in Feb., link:

http://electronicdesign.com/blog/multiprotocol-wireless-soc-targets-iot-connectivity?NL=ED-001&Issue...

We find there is a SiLabs’s Might Gecko wireless SoC supports “The SoC would normally be sleeping, but could periodically wake up to handle 802.15.4 Thread communication and then sub GHz communication

Why can SiLabs’s SoC support this dual-band communication, but KWxx chips cannot? Is this a H/W limitation or S/W issue?

标签 (2)
0 项奖励
回复
1 回复

714 次查看
jc_pacheco
NXP Employee
NXP Employee

KW2xD - 2.4GHz radio

KW20/1Z - 2.4GHz radio

KW01Z - <1 GHz radio

0 项奖励
回复