Can KW2x support ZigBee 868 MHz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can KW2x support ZigBee 868 MHz?

1,568件の閲覧回数
benjaminchang
Contributor V

NXP KW2x is supporting 802.15.4, one of our customer is requesting ZigBee 2.4 GHz and 868 MHz (a GB requirement) since last year. So we proposed KW01Z + KW20Z to them. Checking the new EE Times in Feb., link:

http://electronicdesign.com/blog/multiprotocol-wireless-soc-targets-iot-connectivity?NL=ED-001&Issue...

We find there is a SiLabs’s Might Gecko wireless SoC supports “The SoC would normally be sleeping, but could periodically wake up to handle 802.15.4 Thread communication and then sub GHz communication

Why can SiLabs’s SoC support this dual-band communication, but KWxx chips cannot? Is this a H/W limitation or S/W issue?

ラベル(2)
0 件の賞賛
返信
1 返信

714件の閲覧回数
jc_pacheco
NXP Employee
NXP Employee

KW2xD - 2.4GHz radio

KW20/1Z - 2.4GHz radio

KW01Z - <1 GHz radio

0 件の賞賛
返信