we are running CE DFS test.
for adaptive COT test, we need to issue wifi burst signal command, then will pass the test case.
Is there any burst signal off command for nxp wifi?
thanks
Most of the information related to this process is under "Secure Files" on the page of each NXP device.
The process to retrieve this information is
If you have any questions, please, feel free to ask.
Hi AlanRadirez,
I can not find the document/website.
Could you please tell me the website address or document name?
or attach it to this forum?
Thanks
I cannot provide the file directly or a link to it because it is under a NDA, however, I can provide a guide to get the file.
In https://nxp.com under "My Account" there is a button called "Secure Files"
And then select "Files" and search for DFS
Hi AlanRamirez,
I have found DFS AN, but there is no Burst signal off command information.
We need the command to let burst signal off in order to pass COT test.
Please help to provide the command.
Thanks
Based on my experience, and feedback from the lab, other vendors issue burst off command when running the COT test.
Is there similar command from NXP chipset?
Hello,
Please check the Zero Wait AN for the 88w9098/88Q9098 in the same way that you searched for the first application note
Regards
Does it need to run additional commands in order to pass the COT test?
What are the commands?
The related information as below:
FW: pcieuart9098_combo_v1.bin
Driver: PCIE9098--17.68.1.p109.2-MXM5X17312.p5-GPL-(FP68)