Burst signal off cmd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burst signal off cmd

1,357 Views
Peter17
Contributor I

we are running CE DFS test.

for adaptive COT test, we need to issue wifi burst signal command, then will pass the test case.

Is there any burst signal off command for nxp wifi?

thanks

0 Kudos
Reply
8 Replies

1,308 Views
nxf89619
NXP TechSupport
NXP TechSupport

Most of the information related to this process is under "Secure Files" on the page of each NXP device.
The process to retrieve this information is

  1. Go to the desired NXP device (for example, 88W9098)
  2. Scroll down to "Documentation"
  3. Select "Secure Files"
  4. Search for "DFS AN" or "DFS Application Note"

If you have any questions, please, feel free to ask.

0 Kudos
Reply

1,302 Views
Peter17
Contributor I

Hi AlanRadirez,
I can not find the document/website.
Could you please tell me the website address or document name?

or attach it to this forum?

Thanks

0 Kudos
Reply

1,288 Views
nxf89619
NXP TechSupport
NXP TechSupport

I cannot provide the file directly or a link to it because it is under a NDA, however, I can provide a guide to get the file.

In https://nxp.com under "My Account" there is a button called "Secure Files"

Secure Files button.png

 

 

 

 

And then select "Files" and search for DFS

Search files.png

 

 

 

0 Kudos
Reply

1,270 Views
Peter17
Contributor I

Hi AlanRamirez,

I have found DFS AN, but there is no Burst signal off command information.

We need the command to let burst signal off in order to pass COT test.

Please help to provide the command.

Thanks

0 Kudos
Reply

1,244 Views
Matt3
Contributor I

Based on my experience, and feedback from the lab, other vendors issue burst off command when running the COT test. 
Is there similar command from NXP chipset?

 

0 Kudos
Reply

1,203 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Please check the Zero Wait AN for the 88w9098/88Q9098 in the same way that you searched for the first application note

 

Regards

0 Kudos
Reply

1,318 Views
Matt3
Contributor I

Does it need to run additional commands in order to pass the COT test?

What are the commands?

0 Kudos
Reply

1,336 Views
Peter17
Contributor I

The related information as below:
FW: pcieuart9098_combo_v1.bin
Driver: PCIE9098--17.68.1.p109.2-MXM5X17312.p5-GPL-(FP68)

0 Kudos
Reply