AFLP5G25641 maximum CW output power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AFLP5G25641 maximum CW output power

555 次查看
rflaboratoryoff
Contributor I

I find the AFLP5G25641 very interesting.

I would like to find somehow what would be the maximum output power in CW mode (no pulsed)  for this device.

Thank you very much,

Cristian

标记 (1)
0 项奖励
回复
1 回复

519 次查看
LPP
NXP Employee
NXP Employee

AFLP5G25641 1dB compression power is 29dBm.
Typical average power is about 19.1-20dBm.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复