Hello,
I'm trying to update bt power class of the 88w8987 and I haven't succeed yet.
Their is no information in the datasheet and labtool is still failing.
What can I do ?
Best,
Eric Delanghe
eric.delanghe@faurecia.com
btmon log |
---|
@ RAW Open: labtool (privileged) version 2.22 {0x0004} [hci1] 1086.933839 < HCI Command: Vendor (0x3f|0x0200) plen 16 #246 [hci1] 1091.805552 10 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00 . .............. > HCI Event: Command Complete (0x0e) plen 4 #247 [hci1] 1091.817983 Vendor (0x3f|0x0200) ncmd 1 Status: Unknown HCI Command (0x01) < HCI Command: Vendor (0x3f|0x0200) plen 16 #248 [hci1] 1098.893864 10 20 00 00 01 00 00 00 00 00 00 00 01 00 00 00 . .............. > HCI Event: Command Complete (0x0e) plen 4 #249 [hci1] 1098.904827 Vendor (0x3f|0x0200) ncmd 1 Status: Unknown HCI Command (0x01) < HCI Command: Vendor (0x3f|0x0200) plen 16 #250 [hci1] 1100.869452 10 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00 . .............. > HCI Event: Command Complete (0x0e) plen 4 #251 [hci1] 1100.883948 Vendor (0x3f|0x0200) ncmd 1 Status: Unknown HCI Command (0x01) @ RAW Close: labtool {0x0004} [hci1] 1107.677318 |
Labtool logs |
---|
Name: Dut labtool Version: 1.0.0.146 Date: Jan 20 2020 (14:54:03)Note: 1. =========WiFi tool============= 2. =========BT tool=============Enter CMD 99 to ExitEnter option: 2 Name: DutApiClass Interface: Version: 1.0.0.146 Date: Jan 20 2020 (14:54:03)Note: Initialize drvwrapper for BT .... Dut_Bt_OpenDevice: 0x00000000 ----------------------------------------------------------------------- W87xx (BT) TEST MENU ----------------------------------------------------------------------- Enter option: 113 113 Dut_Bt_GetBtPwrControlClass: 0x00000001 Power Control Class Mode 0 Enter option: 114 1 114 1 Dut_Bt_SetBtPwrControlClass: 0x00000001 Enter option: 113 113 Dut_Bt_GetBtPwrControlClass: 0x00000001 Power Control Class Mode 0 Enter option: 99 99Exiting De-Initialize drvwrapper for BT.... 1. =========WiFi tool============= 2. =========BT tool=============Enter CMD 99 to ExitEnter option: 99 Exiting |
Dear customer,
Which SW release package you're using? Is it MFG fw, or production fw? Cause the production fw doesn't support labtool at all. Also please share the driver/fw loading logs(dmesg) to check if they're loaded successfully.
Thanks,
Ying