88W9098 driver p149, muart_src missing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88W9098 driver p149, muart_src missing?

Jump to solution
543 Views
CupOfTea
Contributor II

The latest driver download for 88W9098 is p149: PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p149.8-17.26.1.p149.8-MXM5X17405_P4_V0V1-GPL.zip

When I extract this package, there doesn't seem to be a tarball that yields muart_src.

When I look at the p136: PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p136.54-17.26.1.p136.54-MXM5X17366_P30_V0V1-GPL.zip

It has a tarball UART-U16-X86-17.26.1.p136-2.2-M3X14100-GPL-src.tgz, which yields muart_src. Such tarball is not found from p149 download.

 

Is this an oversight in p149 packaging? Or is the muart source going to be delivered in some other download going forward.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
514 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @CupOfTea 

 

NXP has taken decision stop providing UART driver. Customer shall use the UART driver from Linux kernel (open source) itself.

 

Regards,

Olivier

View solution in original post

1 Reply
515 Views
ocourson
NXP TechSupport
NXP TechSupport

Dear @CupOfTea 

 

NXP has taken decision stop providing UART driver. Customer shall use the UART driver from Linux kernel (open source) itself.

 

Regards,

Olivier