Hi NXP team,
Using the PAN9028(88W8987) WIFI-BT combo module with the chipset of NXP88W8987 in the Imx8qxp board. We are trying to bring up the WIFI/BT with software package provided by the NXP. (SDIO_WLAN_UART_BT_8987_16.92.21.p18.1_16.92.21.p18.1-LINUX-ANDROID-MM5X17292.p4-MGPL). In SDIO-UART mode, using serial mode combo firmware got downloaded once the bus driver detects the modules SDIO interface. WLAN FW is active and after the hardware initialization the firmware is running on the module, interfaces are registered as wlan0, wlan1 and p2p0. But we are facing a "ForceRegionRule is set in the on-chip OTP memory , call regulatory_set_wiphy_regd US, 11D: Error setting domain info in FW" scenario after firmware is active. Also we got issue like "cmd53 read error=-84" after the Force Region rule. Whole driver seems to crash.
While testing wifi STA/AP mode scan is failing and wifi is not working. Attached the log below and attached it as text file. Please let me know how to solve this region and CMD53 issue.
Note: BT is not tested yet.
Android version used:
Software Package Release Version Information:
Firmware Image used:
Boot log:
4-4817-b71b-b1613620bee1 androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked androidboot.vbmet
a.hash_alg=sha256 androidboot.vbmeta.size=3456 androidboot.vbmeta.digest=0216fd56eefa93fe229
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1500492K/1880956K available (19644K kernel code, 1898K rwdata, 10356K rodata, 4416K init, 587K bss, 85552K reserved, 294912K cma-
reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] random: get_random_bytes called from start_kernel+0x1e0/0x3a4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008853] Console: colour dummy device 80x25
[ 0.013036] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.023214] pid_max: default: 32768 minimum: 301
[ 0.027903] LSM: Security Framework initializing
[ 0.032452] SELinux: Initializing.
[ 0.035970] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.043289] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.052692] ASID allocator initialised with 32768 entries
[ 0.057895] rcu: Hierarchical SRCU implementation.
[ 0.065101] EFI services will not be available.
[ 0.069579] smp: Bringing up secondary CPUs ...
[ 0.074626] Detected VIPT I-cache on CPU1
[ 0.074656] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.074694] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[ 0.074796] smp: Brought up 1 node, 2 CPUs
[ 0.095946] SMP: Total of 2 processors activated.
[ 0.100627] CPU features: detected: 32-bit EL0 Support
[ 0.105772] CPU features: detected: CRC32 instructions
[ 0.110913] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.119231] CPU: All CPU(s) started at EL2
[ 0.123314] alternatives: patching kernel code
[ 0.129015] CPU1: update max cpu_capacity 1024
[ 0.129601] devtmpfs: initialized
[ 0.132847] CPU0: update max cpu_capacity 1024
[ 0.160584] Initilizing CustomIPI irq domain
[ 0.164572] Registered cp15_barrier emulation handler
[ 0.169565] Registered setend emulation handler
[ 0.174473] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.183894] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.200860] pinctrl core: initialized pinctrl subsystem
[ 0.206940] DMI not present or invalid.
[ 0.210966] NET: Registered protocol family 16
[ 0.215912] schedtune: configured to support 5 boost groups
[ 0.230760] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.236572] audit: initializing netlink subsys (disabled)
[ 0.242242] audit: type=2000 audit(0.176:1): state=initialized audit_enabled=0 res=1
[ 0.249691] cpuidle: using governor menu
[ 0.254427] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.262840] Serial: AMBA PL011 UART driver
[ 0.266696] imx mu driver is registered.
[ 0.270519] imx rpmsg driver is registered.
[ 0.275451] printk: console [pstore-1] enabled
[ 0.279809] pstore: Registered ramoops as persistent store backend
[ 0.285729] ramoops: using 0x100000@0x91f00000, ecc: 0
[ 0.389859] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.396239] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.402918] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.409609] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.417602] cryptd: max_cpu_qlen set to 1000
[ 0.426853] ACPI: Interpreter disabled.
[ 0.433295] iommu: Default domain type: Translated
[ 0.438043] vgaarb: loaded
[ 0.440897] SCSI subsystem initialized
[ 0.444758] usbcore: registered new interface driver usbfs
[ 0.449968] usbcore: registered new interface driver hub
[ 0.455284] usbcore: registered new device driver usb
[ 0.462844] mc: Linux media interface: v0.10
[ 0.466838] videodev: Linux video capture interface: v2.00
[ 0.472325] pps_core: LinuxPPS API ver. 1 registered
[ 0.477206] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.486341] PTP clock support registered
[ 0.491039] trusty trusty: failed to get version: -1
[ 0.495682] trusty trusty: selected api version: 0 (requested 3)
[ 0.551849] EDAC MC: Ver: 3.0.0
[ 0.557004] FPGA manager framework
[ 0.560207] Advanced Linux Sound Architecture Driver Initialized.
[ 0.567161] Bluetooth: Core ver 2.22
[ 0.570442] NET: Registered protocol family 31
[ 0.574836] Bluetooth: HCI device and connection manager initialized
[ 0.581182] Bluetooth: HCI socket layer initialized
[ 0.586046] Bluetooth: L2CAP socket layer initialized
[ 0.591084] Bluetooth: SCO socket layer initialized
[ 0.597526] imx-scu scu: NXP i.MX SCU Initialized
[ 0.637601] random: fast init done
[ 0.705553] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/tun1grp
[ 0.714654] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/fec2grp
[ 0.724656] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/ioexp_rst_grp
[ 0.735159] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/mipi_lvds1_pwm_grp
[ 0.745591] imx8qxp-pinctrl scu:pinctrl: no fsl,pins and pins property in node /scu/pinctrl/typecgrp
[ 0.754868] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[ 0.764696] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/lcdifpwmgrp
[ 0.774451] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.788627] clocksource: Switched to clocksource arch_sys_counter
[ 0.884700] VFS: Disk quotas dquot_6.6.0
[ 0.888353] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.895383] pnp: PnP ACPI: disabled
[ 0.933590] thermal_sys: Registered thermal governor 'step_wise'
[ 0.933596] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.939822] NET: Registered protocol family 2
[ 0.950889] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.959135] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.967126] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.974527] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.980901] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.987539] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.994772] NET: Registered protocol family 1
[ 0.999475] PCI: CLS 0 bytes, default 64
[ 1.003356] Trying to unpack rootfs image as initramfs...
[ 1.366700] Freeing initrd memory: 7124K
[ 1.371400] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.380160] kvm [1]: IPA Size Limit: 40bits
[ 1.385143] kvm [1]: GICv3: no GICV resource entry
[ 1.389621] kvm [1]: disabling GICv2 emulation
[ 1.394032] kvm [1]: GIC system register CPU interface enabled
[ 1.399916] kvm [1]: vgic interrupt IRQ1
[ 1.403865] kvm [1]: Hyp mode initialized successfully
[ 1.413397] Initialise system trusted keyrings
[ 1.417663] workingset: timestamp_bits=44 max_order=19 bucket_order=0
[ 1.431833] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.437506] Registering sdcardfs 0.1
[ 1.441162] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.447489] fuse: init (API version 7.31)
[ 1.451547] 9p: Installing v9fs 9p2000 file system support
[ 1.476281] Key type asymmetric registered
[ 1.480055] Asymmetric key parser 'x509' registered
[ 1.484951] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 242)
[ 1.492305] io scheduler mq-deadline registered
[ 1.496815] io scheduler kyber registered
[ 1.524013] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 1.533621] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 1.545858] clock-hsio-refb: gpio_clk_driver_probe: Can't get 'enable' named GPIO property
[ 1.553840] gpio-clk: probe of bus@5f000000:clock-hsio-refb failed with error -2
[ 1.566669] imx8qxp-lpcg-clk 37620000.clock-controller: failed to get clock parent names
[ 1.574535] imx8qxp-lpcg-clk: probe of 37620000.clock-controller failed with error -22
[ 1.664758] mxs-dma 5b810000.dma-apbh: initialized
[ 1.673247] Bus freq driver module loaded
[ 1.684405] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.696592] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 60, base_baud = 5000000) is a FSL_LPUAR[ 1.705777] printk: console [ttyLP0] enabled
[ 1.705777] printk: console [ttyLP0] enabled
[ 1.714208] printk: bootconsole [lpuart32] disabled
[ 1.714208] printk: bootconsole [lpuart32] disabled
[ 1.724311] fsl-lpuart 5a060000.serial: DMA tx channel request failed, operating without tx DMA
[ 1.733080] fsl-lpuart 5a060000.serial: DMA rx channel request failed, operating without rx DMA
[ 1.742503] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 61, base_baud = 5000000) is a FSL_LPUART
[ 1.752974] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 62, base_baud = 5000000) is a FSL_LPUART
[ 1.763436] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 63, base_baud = 5000000) is a FSL_LPUART
[ 1.815909] dpu-core 56180000.dpu: driver probed
[ 1.848045] brd: module loaded
[ 1.859705] loop: module loaded
[ 1.863349] zram: Added device: zram0
[ 1.873446] imx ahci driver is registered.
[ 1.888565] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[ 1.895519] spi-nor: probe of spi0.0 failed with error -2
[ 1.904982] libphy: Fixed MDIO Bus: probed
[ 1.910146] tun: Universal TUN/TAP device driver, 1.6
[ 1.915470] CAN device driver interface
[ 1.923856] thunder_xcv, ver 1.0
[ 1.927179] thunder_bgx, ver 1.0
[ 1.930466] nicpf, ver 1.0
[ 1.937929] hclge is initializing
[ 1.941284] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.948525] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.953924] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.961040] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.966917] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.972769] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.978749] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.985729] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.991354] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.999234] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 2.005853] sky2: driver version 1.30
[ 2.012202] PPP generic driver version 2.4.2
[ 2.016746] PPP BSD Compression module registered
[ 2.021476] PPP Deflate Compression module registered
[ 2.026562] PPP MPPE Compression module registered
[ 2.031372] NET: Registered protocol family 24
[ 2.035834] PPTP driver version 0.8.5
[ 2.039826] usbcore: registered new interface driver r8152
[ 2.045361] usbcore: registered new interface driver asix
[ 2.050842] usbcore: registered new interface driver ax88179_178a
[ 2.056984] usbcore: registered new interface driver cdc_ether
[ 2.062872] usbcore: registered new interface driver net1080
[ 2.068586] usbcore: registered new interface driver cdc_subset
[ 2.074558] usbcore: registered new interface driver zaurus
[ 2.080212] usbcore: registered new interface driver cdc_ncm
[ 2.086146] VFIO - User Level meta-driver version: 0.3
[ 2.098642] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.105223] ehci-pci: EHCI PCI platform driver
[ 2.109770] ehci-platform: EHCI generic platform driver
[ 2.115834] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.122038] ohci-pci: OHCI PCI platform driver
[ 2.126570] ohci-platform: OHCI generic platform driver
[ 2.134249] usbcore: registered new interface driver uas
[ 2.139652] usbcore: registered new interface driver usb-storage
[ 2.145776] usbcore: registered new interface driver usbserial_generic
[ 2.152345] usbserial: USB Serial support registered for generic
[ 2.158398] usbcore: registered new interface driver ftdi_sio
[ 2.164202] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.171568] usbcore: registered new interface driver usb_serial_simple
[ 2.178135] usbserial: USB Serial support registered for carelink
[ 2.184263] usbserial: USB Serial support registered for zio
[ 2.190005] usbserial: USB Serial support registered for funsoft
[ 2.196088] usbserial: USB Serial support registered for flashloader
[ 2.202475] usbserial: USB Serial support registered for google
[ 2.208440] usbserial: USB Serial support registered for libtransistor
[ 2.215064] usbserial: USB Serial support registered for vivopay
[ 2.221342] usbserial: USB Serial support registered for moto_modem
[ 2.227826] usbserial: USB Serial support registered for motorola_tetra
[ 2.234976] usbserial: USB Serial support registered for novatel_gps
[ 2.241966] usbserial: USB Serial support registered for hp4x
[ 2.247991] usbserial: USB Serial support registered for suunto
[ 2.254448] usbserial: USB Serial support registered for siemens_mpi
[ 2.261063] usbcore: registered new interface driver usb_ehset_test
[ 2.279418] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 2.287566] usbcore: registered new interface driver xpad
[ 2.293056] usbcore: registered new interface driver usb_acecad
[ 2.299023] usbcore: registered new interface driver aiptek
[ 2.304649] usbcore: registered new interface driver gtco
[ 2.310107] usbcore: registered new interface driver hanwang
[ 2.315820] usbcore: registered new interface driver kbtab
[ 2.324895] imx-sc-rtc scu:rtc: registered as rtc0
[ 2.329794] imx-sc-rtc scu:rtc: setting system clock to 2022-09-10T04:08:13 UTC (1662782893)
[ 2.339705] i2c /dev entries driver
[ 2.347442] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video0 (81,0)
[ 2.357047] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video1 (81,1)
[ 2.366967] uvcvideo: Unable to create debugfs directory
[ 2.372391] usbcore: registered new interface driver uvcvideo
[ 2.378152] USB Video Class driver (1.1.1)
[ 2.384702] __power_supply_register: Expected proper parent device for 'battery'
[ 2.392623] __power_supply_register: Expected proper parent device for 'usb'
[ 2.404204] trusty-log not supported on secure side.
[ 2.409806] trusty-virtio trusty:trusty-virtio: initializing
[ 2.415586] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
[ 2.425085] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr
[ 2.432597] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices
[ 2.442485] device-mapper: uevent: version 1.0.3
[ 2.447466] device-mapper: ioctl: 4.41.0-ioctl (2019-09-16) initialised: dm-devel@redhat.com
[ 2.464490] sdhci: Secure Digital Host Controller Interface driver
[ 2.470715] sdhci: Copyright(c) Pierre Ossman
[ 2.475904] Synopsys Designware Multimedia Card Interface Driver
[ 2.484372] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.492368] mmc0: CQHCI version 5.10
[ 2.501190] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.509101] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.517522] usbcore: registered new interface driver usbhid
[ 2.523121] usbhid: USB HID core driver
[ 2.530653] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 2.538716] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[ 2.564984] mxc-mipi-csi2 58227000.csi: lanes: 2, name: mxc-mipi-csi2.0
[ 2.574313] mxc-parallel-csi 58261000.pcsi: mxc_parallel_csi_probe probe successfully
[ 2.583398] ashmem: initialized
[ 2.602357] Galcore version 6.4.3.p1.305572
[ 2.672474] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu0_ss on minor 0
[ 2.687751] usbcore: registered new interface driver snd-usb-audio
[ 2.737900] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59820000
[ 2.745044] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59830000
[ 2.752484] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59820000.sai mapping ok
[ 2.760136] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> 59830000.sai mapping ok
[ 2.767827] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-0 mapping ok
[ 2.775135] imx-audmix imx-audmix.0: snd-soc-dummy-dai <-> audmix-1 mapping ok
[ 2.782451] imx-audmix imx-audmix.0: ASoC: no DMI vendor name!
[ 2.794590] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.802579] drop_monitor: Initializing network drop monitor service
[ 2.808998] NET: Registered protocol family 26
[ 2.813470] netem: version 1.3
[ 2.816533] u32 classifier
[ 2.819268] input device check on
[ 2.822944] Actions configured
[ 2.827199] xt_time: kernel timezone is -0000
[ 2.831748] gre: GRE over IPv4 demultiplexor driver
[ 2.836643] IPv4 over IPsec tunneling driver
[ 2.841618] Initializing XFRM netlink socket
[ 2.845935] IPsec XFRM device driver
[ 2.850088] NET: Registered protocol family 10
[ 2.855632] Segment Routing with IPv6
[ 2.859424] mip6: Mobile IPv6
[ 2.863516] NET: Registered protocol family 17
[ 2.868040] NET: Registered protocol family 15
[ 2.872503] can: controller area network core (rev 20170425 abi 9)
[ 2.878773] NET: Registered protocol family 29
[ 2.883249] can: raw protocol (rev 20170425)
[ 2.887545] can: broadcast manager protocol (rev 20170425 t)
[ 2.893251] can: netlink gateway (rev 20190810) max_hops=1
[ 2.899026] Bluetooth: RFCOMM TTY layer initialized
[ 2.903959] Bluetooth: RFCOMM socket layer initialized
[ 2.909142] Bluetooth: RFCOMM ver 1.11
[ 2.912914] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.918242] Bluetooth: BNEP filters: protocol multicast
[ 2.923486] Bluetooth: BNEP socket layer initialized
[ 2.928493] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.934437] Bluetooth: HIDP socket layer initialized
[ 2.939465] l2tp_core: L2TP core driver, V2.0
[ 2.943853] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.948658] 8021q: 802.1Q VLAN Support v1.8
[ 2.952896] lib80211: common routines for IEEE802.11 drivers
[ 2.959369] 9pnet: Installing 9P2000 support
[ 2.963728] tsn generic netlink module v1 init...
[ 2.969460] registered taskstats version 1
[ 2.973586] Loading compiled-in X.509 certificates
[ 2.978571] Key type ._fscrypt registered
[ 2.982597] Key type .fscrypt registered
[ 2.986563] Key type fscrypt-provisioning registered
[ 2.992789] pstore: Using crash dump compression: deflate
[ 3.001701] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[ 3.026060] mmc1: CQHCI version 5.10
[ 3.029781] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO
[ 3.066790] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 3.163794] usb_phy_generic bus@5b000000:usb3-phy: bus@5b000000:usb3-phy supply vcc not found, using dummy regulator
[ 3.193093] cs42xx8 16-0048: found device, revision 3
[ 3.198311] i2c i2c-16: LPI2C adapter registered
[ 3.206101] pca954x 17-0071: probe failed
[ 3.210274] i2c i2c-17: LPI2C adapter registered
[ 3.214922] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.225092] i2c i2c-18: LPI2C adapter registered
[ 3.231313] imx8qxp-lpcg-clk 37620000.clock-controller: failed to get clock parent names
[ 3.239626] imx8qxp-lpcg-clk: probe of 37620000.clock-controller failed with error -22
[ 3.304761] mmc0: CQHCI version 5.10
[ 3.310824] pps pps0: new PPS source ptp0
[ 3.322168] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 3.329015] fec 5b040000.ethernet: Using random MAC address: 42:18:3a:5e:ba:f0
[ 3.337940] libphy: fec_enet_mii_bus: probed
[ 3.346112] fec 5b040000.ethernet eth0: registered PHC device 0
[ 3.356502] xhci-cdns3: xHCI Host Controller
[ 3.360927] xhci-cdns3: new USB bus registered, assigned bus number 1
[ 3.368880] xhci-cdns3: hcc params 0x200073c8 hci version 0x100 quirks 0x0000001000018010
[ 3.378382] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 3.387846] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.396115] usb usb1: Product: xHCI Host Controller
[ 3.402181] usb usb1: Manufacturer: Linux 5.4.70-g372a79b85-dirty xhci-hcd
[ 3.410115] usb usb1: SerialNumber: xhci-cdns3
[ 3.423517] hub 1-0:1.0: USB hub found
[ 3.428341] hub 1-0:1.0: 1 port detected
[ 3.437784] xhci-cdns3: xHCI Host Controller
[ 3.442167] xhci-cdns3: new USB bus registered, assigned bus number 2
[ 3.449802] xhci-cdns3: Host supports USB 3.0 SuperSpeed
[ 3.459353] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.465995] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 3.474706] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 3.479240] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.04
[ 3.487527] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.494768] usb usb2: Product: xHCI Host Controller
[ 3.499667] usb usb2: Manufacturer: Linux 5.4.70-g372a79b85-dirty xhci-hcd
[ 3.506562] usb usb2: SerialNumber: xhci-cdns3
[ 3.512295] hub 2-0:1.0: USB hub found
[ 3.516128] hub 2-0:1.0: 1 port detected
[ 3.526219] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12
[ 3.533862] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.540678] [drm] No driver support for vblank timestamp query.
[ 3.547290] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.557068] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.564944] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.574459] imx-rproc imx8x_cm4@0: failed to find syscon
[ 3.580078] imx-rproc imx8x_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[ 3.589429] imx-rproc imx8x_cm4@0: No txdb, ret 0
[ 3.594971] remoteproc remoteproc0: imx-rproc is available
[ 3.602378] pwm-backlight lvds_backlight@0: lvds_backlight@0 supply power not found, using dummy regulator
[ 3.612546] pwm-backlight lvds_backlight@1: lvds_backlight@1 supply power not found, using dummy regulator
[ 3.630351] asoc-simple-card sound-bt-radio: bt-sco-pcm <-> 59040000.sai mapping ok
[ 3.638083] asoc-simple-card sound-bt-radio: ASoC: no DMI vendor name!
[ 3.646358] asoc-simple-card sound-bm23-sco: bt-sco-pcm-wb <-> 59050000.sai mapping ok
[ 3.654359] asoc-simple-card sound-bm23-sco: ASoC: no DMI vendor name!
[ 3.664236] i2c i2c-19: LPI2C adapter registered
[ 4.715582] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.743729] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.771890] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.800048] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.828085] ILITEK ERR line = 425 ilitek_i2c_write_and_read : ilitek_i2c_write_and_read, i2c write error, ret = -5
[ 4.843997] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.872249] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.900402] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.928568] ILITEK ERR line = 353 ilitek_i2c_transfer : ilitek_i2c_transfer err
[ 4.956597] ILITEK ERR line = 432 ilitek_i2c_write_and_read : ilitek_i2c_write_and_read, i2c read error, ret = -5
[ 4.967054] ILITEK ERR line = 1804 ilitek_main_probe : init read tp protocol error so exit
[ 4.975532] ILITEK ERR line = 1877 ilitek_main_probe : return -ENODEV
[ 4.982292] i2c i2c-20: LPI2C adapter registered
[ 4.988843] mmc0: CQHCI version 5.10
[ 4.992521] sdhci-esdhc-imx 5b010000.mmc: allocated mmc-pwrseq
[ 5.030010] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 5.039846] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 5.050983] [drm] No driver support for vblank timestamp query.
[ 5.057004] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 5.070008] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 5.077584] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 5.085617] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[ 5.094153] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 5.102512] imx-drm display-subsystem: bound 56248000.dsi_host (ops nwl_dsi_component_ops)
[ 5.111233] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 5.161243] mmc0: new high speed SDIO card at address 0001
[ 5.234850] Console: switching to colour frame buffer device 128x37
[ 5.265486] imx-drm display-subsystem: fb0: imx-drmdrmfb frame buffer device
[ 5.281347] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 5.291516] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 5.303366] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 5.310132] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 5.318907] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 5.351488] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 5.358200] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 5.364688] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 5.371595] mx8-img-md: Unregistered all entities
[ 5.440712] imx-cs42888 sound-cs42888: cs42888 <-> 59010000.esai mapping ok
[ 5.451421] imx-cs42888 sound-cs42888: snd-soc-dummy-dai <-> 59000000.asrc mapping ok
[ 5.459529] imx-cs42888 sound-cs42888: cs42888 <-> 59010000.esai mapping ok
[ 5.466647] imx-cs42888 sound-cs42888: ASoC: no DMI vendor name!
[ 5.485916] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 5.485918] ALSA device list:
[ 5.485926] #0: imx-audmix
[ 5.492541] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 5.495218] #1: radio
[ 5.495221] #2: bm23-sco-audio
[ 5.495224] #3: imx-cs42888
[ 5.513391] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 5.515275] Freeing unused kernel memory: 4416K
[ 5.520382] mx8-img-md: Unregistered all entities
[ 5.540703] Run /init as init process
[ 5.598088] init: init first stage started!
[ 5.602749] init: Switching root to '/first_stage_ramdisk'
[ 5.611757] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 5.673890] init: [libfs_mgr]Created logical partition system_a on device /dev/block/dm-0
[ 5.682143] init: [libfs_mgr]Skipping zero-length logical partition: system_b
[ 5.690458] init: [libfs_mgr]Created logical partition vendor_a on device /dev/block/dm-1
[ 5.698720] init: [libfs_mgr]Skipping zero-length logical partition: vendor_b
[ 5.707000] init: [libfs_mgr]Created logical partition product_a on device /dev/block/dm-2
[ 5.715370] init: [libfs_mgr]Skipping zero-length logical partition: product_b
[ 5.735723] init: [libfs_avb]Returning avb_handle with status: Success
[ 5.747777] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 5.767881] EXT4-fs (dm-3): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 5.796122] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 5.815967] EXT4-fs (dm-4): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 5.829402] device-mapper: verity: sha1 using implementation "sha1-ce"
[ 5.853710] EXT4-fs (dm-5): mounted filesystem without journal. Opts: errors=panic,barrier=1,inode_readahead_blks=8
[ 5.908718] printk: init: 16 output lines suppressed due to ratelimiting
[ 5.939705] random: init: uninitialized urandom read (40 bytes read)
[ 6.200201] random: init: uninitialized urandom read (40 bytes read)
[ 6.239384] init: Loading SELinux policy
[ 6.311869] SELinux: Permission nlmsg_readpriv in class netlink_route_socket not defined in policy.
[ 6.321723] SELinux: the above unknown classes and permissions will be denied
[ 6.328965] SELinux: policy capability network_peer_controls=1
[ 6.334925] SELinux: policy capability open_perms=1
[ 6.339919] SELinux: policy capability extended_socket_class=1
[ 6.346015] SELinux: policy capability always_check_network=0
[ 6.351904] SELinux: policy capability cgroup_seclabel=0
[ 6.357325] SELinux: policy capability nnp_nosuid_transition=1
[ 6.499402] audit: type=1403 audit(1662782897.664:2): auid=4294967295 ses=4294967295 lsm=selinux res=1
[ 6.499847] selinux: SELinux: Loaded policy from /vendor/etc/selinux/precompiled_sepolicy
[ 6.499847]
[ 6.534432] selinux: SELinux: Loaded file_contexts
[ 6.534432]
[ 6.551024] random: init: uninitialized urandom read (40 bytes read)
[ 6.619373] init: init second stage started!
[ 6.674126] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 6.691089] selinux: SELinux: Loaded file_contexts
[ 6.691089]
[ 6.697457] init: Running restorecon...
[ 6.733416] init: Overriding previous 'ro.' property 'pm.dexopt.boot':'verify' with new value 'quicken'
[ 6.748214] init: Couldn't load property file '/product_services/build.prop': open() failed: No such file or directory: No such file or directory
[ 6.761394] init: Couldn't load property file '/factory/factory.prop': open() failed: No such file or directory: No such file or directory
[ 6.777540] init: Setting product property ro.product.brand to 'Android' (from ro.product.product.brand)
[ 6.787123] init: Setting product property ro.product.device to 'mek_8q' (from ro.product.product.device)
[ 6.796819] init: Setting product property ro.product.manufacturer to 'freescale' (from ro.product.product.manufacturer)
[ 7.009193] urandom_read: 5 callbacks suppressed
[ 7.009203] random: ueventd: uninitialized urandom read (40 bytes read)
[ 7.020009] random: apexd: uninitialized urandom read (40 bytes read)
[ 7.085050] ueventd: ueventd started!
[ 7.094691] selinux: SELinux: Loaded file_contexts
[ 7.094691]
[ 7.101423] ueventd: Parsing file /ueventd.rc...
[ 7.112266] ueventd: Parsing file /vendor/ueventd.rc...
[ 7.123451] ueventd: Parsing file /odm/ueventd.rc...
[ 7.128592] ueventd: Unable to read config file '/odm/ueventd.rc': open() failed: No such file or directory
[ 7.138546] ueventd: Parsing file /ueventd.freescale.rc...
[ 7.144189] ueventd: Unable to read config file '/ueventd.freescale.rc': open() failed: No such file or directory
[ 7.144381] apexd: Bootstrap subcommand detected
[ 7.573380] ueventd: firmware: loading 'regulatory.db' for '/devices/platform/regulatory.0/firmware/regulatory.db'
[ 7.601551] ueventd: loading /devices/platform/regulatory.0/firmware/regulatory.db took 28ms
[ 7.656483] apexd: wait for '/dev/loop-control' took 451ms
[ 7.662828] apexd: Pre-allocated 9 loopback devices
[ 7.681402] apexd: Scanning /system/apex for embedded keys
[ 7.691851] apexd: Scanning /product/apex for embedded keys
[ 7.706499] apexd: ... does not exist. Skipping
[ 7.716491] apexd: Scanning /system/apex looking for APEX packages.
[ 7.723623] apexd: Found /system/apex/com.android.conscrypt.apex
[ 7.730504] apexd: Skipped when bootstrapping
[ 7.734962] apexd: Found /system/apex/com.android.apex.cts.shim.apex
[ 7.806510] EXT4-fs (loop0): mounted filesystem without journal. Opts: (null)
[ 7.893953] EXT4-fs (loop1): mounted filesystem without journal. Opts: (null)
[ 7.909213] printk: apexd: 13 output lines suppressed due to ratelimiting
[ 7.923361] audit: type=1400 audit(1662782899.088:3): avc: denied { write } for pid=186 comm="init" name="/" dev="tmpfs" ino=1528 scontext=u:r:ven
dor_init:s0 tcontext=u:object_r:tmpfs:s0 tclass=dir permissive=1
[ 7.942463] audit: type=1400 audit(1662782899.088:4): avc: denied { add_name } for pid=186 comm="init" name="usb1" scontext=u:r:vendor_init:s0 tco
ntext=u:object_r:tmpfs:s0 tclass=dir permissive=1
[ 7.960399] audit: type=1400 audit(1662782899.088:5): avc: denied { create } for pid=186 comm="init" name="usb1" scontext=u:r:vendor_init:s0 tcont
ext=u:object_r:tmpfs:s0 tclass=dir permissive=1
[ 8.060894] Registered swp emulation handler
[ 8.099091] Console: switching to colour dummy device 80x25
[ 8.178757] watchdogd: watchdogd started (interval 10, margin 20)!
[ 8.237763] EXT4-fs (mmcblk1p6): Ignoring removed nomblk_io_submit option
[ 8.280876] logd.auditd: start
[ 8.283985] logd.klogd: 8111356125
[ 8.305411] EXT4-fs (mmcblk1p6): recovery complete
[ 8.319333] EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
[ 8.336931] ext4 filesystem being mounted at /metadata supports timestamps until 2038 (0x7fffffff)
[ 8.447212] wlan: Loading MWLAN driver
[ 8.458114] wlan: Driver loaded successfully
[ 8.460007] wlan: Register to Bus Driver...
[ 8.472829] vendor=0x02DF device=0x9149 class=0 function=1
[ 8.479084] Attach moal handle ops, card interface type: 0x105
[ 8.486697] SD8987: init module param from usr cfg
[ 8.491675] card_type: SD8987, config block: 0
[ 8.496235] cfg80211_wext=0xf
[ 8.499347] sta_name=wlan
[ 8.502089] uap_name=wlan
[ 8.504770] wfd_name=p2p
[ 8.507445] max_vir_bss=1
[ 8.510261] cal_data_cfg=none
[ 8.513367] ps_mode = 2
[ 8.515867] auto_ds = 2
[ 8.518419] fw_name=sduart8987_combo.bin
[ 8.523100] SDIO: max_segs=128 max_seg_size=65535
[ 8.527943] rx_work=1 cpu_num=2
[ 8.531224] Attach mlan adapter operations.card_type is 0x105.
[ 8.537790] wlan: Enable TX SG mode
[ 8.541358] wlan: Enable RX SG mode
[ 8.552816] Request firmware: sduart8987_combo.bin
[ 8.555772] e2fsck: e2fsck 1.44.4 (18-Aug-2018)
[ 8.555772]
[ 8.573037] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[ 8.573037]
[ 8.592242] HCI UART driver ver 2.2-M2614100
[ 8.594121] HCI H4 protocol initialized
[ 8.596594] e2fsck: Pass 2: Checking directory structure
[ 8.596594]
[ 8.598489] HCI BCSP protocol initialized
[ 8.602521] e2fsck: Pass 3: Checking directory connectivity
[ 8.602521]
[ 8.609161] HCILL protocol initialized
[ 8.613352] e2fsck: Pass 4: Checking reference counts
[ 8.613352]
[ 8.630998] e2fsck: Pass 5: Checking group summary information
[ 8.630998]
[ 8.638660] e2fsck: metadata: 17/256 files (5.9% non-contiguous), 1102/2048 blocks
[ 8.638660]
[ 8.655981] EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: discard
[ 8.667580] ext4 filesystem being mounted at /metadata supports timestamps until 2038 (0x7fffffff)
[ 8.679940] g_serial gadget: Gadget Serial v2.4
[ 8.685002] g_serial gadget: g_serial ready
[ 8.912942] random: crng init done
[ 8.953164] zram0: detected capacity change from 0 to 629145600
[ 9.072589] Wlan: FW download over, firmwarelen=579232 downloaded 579232
[ 9.085618] mkswap: Swapspace size: 614396k, UUID=534cc390-a5f7-4c9f-8524-3d1cf4a1daf3
[ 9.116760] Adding 614396k swap on /dev/block/zram0. Priority:-2 extents:1 across:614396k SS
[ 9.128019] type=1400 audit(1662782900.292:6): avc: denied { write } for comm="init" name="enforce" dev="selinuxfs" ino=4 scontext=u:r:vendor_init:s0
tcontext=u:object_r:selinuxfs:s0 tclass=file permissive=1
[ 9.296362] type=1400 audit(1662782900.292:6): avc: denied { write } for comm="init" name="enforce" dev="selinuxfs" ino=4 scontext=u:r:vendor_init:s0
tcontext=u:object_r:selinuxfs:s0 tclass=file permissive=1
[ 9.315047] type=1400 audit(1662782900.460:7): avc: denied { search } for comm="android.hardwar" name="/" dev="mmcblk1p6" ino=2 scontext=u:r:hal_boot
ctl_default:s0 tcontext=u:object_r:metadata_file:s0 tclass=dir permissive=1
[ 9.335738] type=1400 audit(1662782900.460:7): avc: denied { search } for comm="android.hardwar" name="/" dev="mmcblk1p6" ino=2 scontext=u:r:hal_boot
ctl_default:s0 tcontext=u:object_r:metadata_file:s0 tclass=dir permissive=1
[ 9.355858] type=1400 audit(1662782900.460:8): avc: denied { search } for comm="android.hardwar" name="gsi" dev="mmcblk1p6" ino=16 scontext=u:r:hal_b
ootctl_default:s0 tcontext=u:object_r:gsi_metadata_file:s0 tclass=dir permissive=1
[ 9.382461] EXT4-fs (mmcblk1p9): Ignoring removed nomblk_io_submit option
[ 9.623906] EXT4-fs (mmcblk1p9): 1 orphan inode deleted
[ 9.629589] EXT4-fs (mmcblk1p9): recovery complete
[ 9.651410] EXT4-fs (mmcblk1p9): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
[ 10.156755] WLAN FW is active
[ 10.159758] on_time is 9987154125
[ 10.201368] fw_cap_info=0x181c3f03, dev_cap_mask=0xffffffff
[ 10.207005] max_p2p_conn = 8, max_sta_conn = 8
[ 10.231455] e2fsck: e2fsck 1.44.4 (18-Aug-2018)
[ 10.231455]
[ 10.240770] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[ 10.240770]
[ 10.249314] e2fsck: Pass 2: Checking directory structure
[ 10.249314]
[ 10.259799] e2fsck: Pass 3: Checking directory connectivity
[ 10.259799]
[ 10.270544] e2fsck: Pass 4: Checking reference counts
[ 10.270544]
[ 10.282052] e2fsck: Pass 5: Checking group summary information
[ 10.282052]
[ 10.292896] e2fsck: userdata: 1851/383520 files (2.2% non-contiguous), 50665/1531904 blocks
[ 10.292896]
[ 10.305118] EXT4-fs (mmcblk1p9): Ignoring removed nomblk_io_submit option
[ 10.328294] EXT4-fs (mmcblk1p9): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
[ 10.465482] ForceRegionRule is set in the on-chip OTP memory
[ 10.466282] call regulatory_set_wiphy_regd US
[ 10.466287] ------------[ cut here ]------------
[ 10.471199] 11D: Error setting domain info in FW
[ 10.471210] ForceRegionRule is set in the on-chip OTP memory
[ 10.475813] Invalid regulatory domain detected
[ 10.480198] 11D: Error setting domain info in FW
[ 10.499926] WARNING: CPU: 0 PID: 247 at /home/AMR/android_build/vendor/nxp-opensource/kernel_imx/net/wireless/reg.c:3723 __regulatory_set_wiphy_
regd+0x190/0x1a0
[ 10.514719] Modules linked in: g_serial hci_uart moal mlan
[ 10.520222] CPU: 0 PID: 247 Comm: kworker/u5:2 Not tainted 5.4.70-g372a79b85-dirty #1649
[ 10.528312] Hardware name: Freescale i.MX8DX MEK (DT)
[ 10.533420] Workqueue: MOAL_EVT_WORK_QUEUE woal_regulatory_work_queue [moal]
[ 10.540477] pstate: 60400005 (nZCv daif +PAN -UAO)
[ 10.545273] pc : __regulatory_set_wiphy_regd+0x190/0x1a0
[ 10.550589] lr : __regulatory_set_wiphy_regd+0x18c/0x1a0
[ 10.555903] sp : ffff8000135dbcb0
[ 10.559222] x29: ffff8000135dbcd0 x28: 0000000000000035
[ 10.564538] x27: ffff000065f24000 x26: ffff000065f241f0
[ 10.569855] x25: ffff000065b3b078 x24: ffff000065b3b070
[ 10.575172] x23: ffff8000094bcda7 x22: 0000000000000004
[ 10.580488] x21: ffff8000094c3000 x20: ffff00006529e3e0
[ 10.585805] x19: ffff000065f24000 x18: 0000000304b13324
[ 10.591122] x17: 0000000000000400 x16: ffff0000663710a0
[ 10.596439] x15: 0000000000000001 x14: 0000000000005c54
[ 10.601755] x13: 0000000000000000 x12: ffff800011f92060
[ 10.607071] x11: 0000000000000000 x10: 0000000000000000
[ 10.612389] x9 : 1f84faaaacb4f400 x8 : 1f84faaaacb4f400
[ 10.617706] x7 : 0000000000000100 x6 : 0000000000000000
[ 10.623023] x5 : ffff80001319bce0 x4 : 0000000000000004
[ 10.628339] x3 : 0000000000000000 x2 : ffff00006dbb6800
[ 10.633656] x1 : ffff00006dba6398 x0 : ffff000065f24000
[ 10.638973] Call trace:
[ 10.641427] __regulatory_set_wiphy_regd+0x190/0x1a0
[ 10.646396] regulatory_set_wiphy_regd_sync_rtnl+0x34/0x78
[ 10.651916] woal_regulatory_work_queue+0x41c/0x550 [moal]
[ 10.657414] process_one_work+0x214/0x470
[ 10.661424] worker_thread+0x32c/0x4b8
[ 10.665177] kthread+0x138/0x148
[ 10.668411] ret_from_fork+0x10/0x18
[ 10.671986] ---[ end trace 478c436a95eccba6 ]---
[ 10.676976] ForceRegionRule is set in the on-chip OTP memory
[ 10.682952] 11D: Error setting domain info in FW
[ 10.687924] ForceRegionRule is set in the on-chip OTP memory
[ 10.693756] 11D: Error setting domain info in FW
[ 10.705185] ForceRegionRule is set in the on-chip OTP memory
[ 10.711115] 11D: Error setting domain info in FW
[ 10.715858] ForceRegionRule is set in the on-chip OTP memory
[ 10.723686] 11D: Error setting domain info in FW
[ 10.731625] wlan: version = SD8987----16.92.10.p208-MM5X16292.p4-GPL-(FP92)
[ 10.739140] Set REG 0x80002328: 0x13d57 slew_rate=3
[ 10.744652] cmd53 read error=-84
[ 10.752878] wlan: cmd53 read regs failed: -1 port=0 retry=0
[ 10.762355] cmd53 read error=-84
[ 10.765795] wlan: cmd53 read regs failed: -1 port=0 retry=1
[ 10.771629] cmd53 read error=-84
[ 10.775222] wlan: cmd53 read regs failed: -1 port=0 retry=2
[ 10.780976] wlan: Fail to read mp_regs
[ 10.813807] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
[ 10.954827] fscrypt: AES-256-XTS using implementation "xts-aes-ce"
[ 10.980884] apexd: Marking APEXd as starting
[ 10.987353] apexd: Scanning /system/apex for embedded keys
[ 11.000132] apexd: Scanning /product/apex for embedded keys
[ 11.093052] EXT4-fs (loop2): mounted filesystem without journal. Opts: (null)
[ 11.141741] init (pid 1) is setting deprecated v1 encryption policy; recommend upgrading to v2.
[ 11.186917] EXT4-fs (loop3): mounted filesystem without journal. Opts: (null)
[ 11.286724] EXT4-fs (loop4): mounted filesystem without journal. Opts: (null)
[ 11.367168] EXT4-fs (loop5): mounted filesystem without journal. Opts: (null)
[ 11.450244] EXT4-fs (loop6): mounted filesystem without journal. Opts: (null)
[ 11.530385] EXT4-fs (loop7): mounted filesystem without journal. Opts: (null)
[ 11.623512] EXT4-fs (loop8): mounted filesystem without journal. Opts: (null)
[ 11.637431] init: Wait for property 'apexd.status=ready' took 478ms
[ 11.650425] init: Parsing file /apex/com.android.media.swcodec@299900000/etc/init.rc...
[ 11.659829] init: starting service 'exec 6 (/system/bin/vdc --wait cryptfs init_user0)'...
[ 11.670700] init: SVC_EXEC service 'exec 6 (/system/bin/vdc --wait cryptfs init_user0)' pid 294 (uid 0 gid 0+0 context default) started; waiting...
[ 11.866527] init: Service 'exec 6 (/system/bin/vdc --wait cryptfs init_user0)' (pid 294) exited with status 0 waiting took 0.196000 seconds
[ 11.881467] selinux: SELinux: Skipping restorecon on directory(/data)
[ 11.881467]
[ 11.890152] init: starting service 'exec 7 (/system/bin/tzdatacheck /apex/com.android.runtime/etc/tz /data/misc/zoneinfo)'...
[ 11.903961] init: SVC_EXEC service 'exec 7 (/system/bin/tzdatacheck /apex/com.android.runtime/etc/tz /data/misc/zoneinfo)' pid 297 (uid 1000 gid 1000
+0 context default) started; waiting...
[ 11.948945] init: Service 'exec 7 (/system/bin/tzdatacheck /apex/com.android.runtime/etc/tz /data/misc/zoneinfo)' (pid 297) exited with status 0 wait
ing took 0.045000 seconds
[ 11.965422] init: processing action (post-fs-data) from (/init.usb.rc:6)
[ 12.210600] logd.daemon: reinit
[ 12.297522] update_verifier: Started with arg 1: nonencrypted
[ 12.309839] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[ 12.316404] update_verifier: Leaving update_verifier.
[ 12.336075] type=1400 audit(1662782900.460:8): avc: denied { search } for comm="android.hardwar" name="gsi" dev="mmcblk1p6" ino=16 scontext=u:r:hal_b
ootctl_default:s0 tcontext=u:object_r:gsi_metadata_file:s0 tclass=dir permissive=1
[ 12.356796] type=1400 audit(1662782903.500:9): avc: denied { setattr } for comm="init" name="wifi" dev="mmcblk1p9" ino=130595 scontext=u:r:vendor_ini
t:s0 tcontext=u:object_r:wifi_data_file:s0 tclass=dir permissive=1
[ 12.465887] Mass Storage Function, version: 2009/09/11
[ 12.478015] LUN: removable file: (no medium)
[ 12.505643] using random self ethernet address
[ 12.516486] using random host ethernet address
[ 12.551190] file system registered
[ 12.607470] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 12.612701] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 3
[ 12.632699] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 12.638379] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 12.646767] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.654064] usb usb3: Product: EHCI Host Controller
[ 12.659001] usb usb3: Manufacturer: Linux 5.4.70-g372a79b85-dirty ehci_hcd
[ 12.665921] usb usb3: SerialNumber: ci_hdrc.0
[ 12.671289] hub 3-0:1.0: USB hub found
[ 12.675202] hub 3-0:1.0: 1 port detected
[ 12.685740] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 12.713500] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 12.720118] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 12.741343] mx8-img-md: Unregistered all entities
[ 12.756934] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 12.769449] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 12.783666] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 12.791933] mx8-img-md: Unregistered all entities
[ 13.297358] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 14.229653] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
mek_8q:/ $ [ 15.672242] [VPU Encoder] enable mu for core[0]
[ 15.692346] [VPU Encoder] vpu encoder core[0] firmware version is 1.3.0
[ 15.752665] Timeout cmd id (15.580048) = 0x19, act = 0x1
[ 15.758037] 19
[ 15.758040] 00
[ 15.759795] 10
[ 15.761560] 00
[ 15.763310] 22
[ 15.765071] 00
[ 15.766820] 00
[ 15.768566] 00
[ 15.770324] 01
[ 15.772078] 00
[ 15.773854] 28
[ 15.775604] 23
[ 15.777370] 57
[ 15.779121] 3d
[ 15.780880] 01
[ 15.782631] 00
[ 15.784377]
[ 15.787630] BSS type = 0 BSS role= 0
[ 15.791219] ------------Dump info-----------
[ 15.795501] Commmand Timeout
[ 15.798398] mlan_processing =0
[ 15.801460] main_lock_flag =0
[ 15.804430] main_process_cnt =49
[ 15.807672] delay_task_flag =0
[ 15.810738] mlan_rx_processing =0
[ 15.814067] rx_pkts_queued=0
[ 15.816957] more_task_flag = 0
[ 15.820016] num_cmd_timeout = 1
[ 15.823173] last_cmd_index = 4
[ 15.826238] last_cmd_id =
[ 15.826241] 0xe4
[ 15.828956] 0x4d
[ 15.830884] 0xd1
[ 15.832824] 0x19
[ 15.834750] 0x19
[ 15.836689] 0x242
[ 15.838615] 0x4d
[ 15.840641] 0xd1
[ 15.842566] 0xb0
[ 15.844486] 0xd1
[ 15.846417]
[ 15.849842] last_cmd_act =
[ 15.849844] 0x0
[ 15.852645] 0x1
[ 15.854487] 0x0
[ 15.856329] 0x0
[ 15.858184] 0x1
[ 15.860022] 0x0
[ 15.861882] 0x1
[ 15.863721] 0x0
[ 15.865575] 0x1
[ 15.867413] 0x0
[ 15.869264]
[ 15.872593] last_cmd_resp_index = 3
[ 15.876113] last_cmd_resp_id =
[ 15.876116] 0x80e4
[ 15.879299] 0x804d
[ 15.881410] 0x80d1
[ 15.883510] 0x8019
[ 15.885619] 0x80e4
[ 15.887716] 0x8242
[ 15.889834] 0x804d
[ 15.891938] 0x80d1
[ 15.894045] 0x80b0
[ 15.896142] 0x80d1
[ 15.898311]
[ 15.901941] last_event_index = 0
[ 15.905182] last_event =
[ 15.905186] 0x0
[ 15.907812] 0x0
[ 15.909674] 0x0
[ 15.911547] 0x0
[ 15.913432] 0x0
[ 15.915273] 0x0
[ 15.917123] 0x0
[ 15.918965] 0x0
[ 15.920811] 0x0
[ 15.922651] 0x0
[ 15.924489]
[ 15.927849] num_data_h2c_failure = 0
[ 15.931452] num_cmd_h2c_failure = 0
[ 15.935021] num_data_c2h_failure = 0
[ 15.938614] num_cmdevt_c2h_failure = 0
[ 15.942398] num_int_read_failure = 1
[ 15.945997] last_int_status = 192
[ 15.949344] num_alloc_buffer_failure = 0
[ 15.953298] num_pkt_dropped = 0
[ 15.956444] num_no_cmd_node = 0
[ 15.959618] num_event_deauth = 0
[ 15.962871] num_event_disassoc = 0
[ 15.966298] num_event_link_lost = 0
[ 15.969832] num_cmd_deauth = 0
[ 15.972904] num_cmd_assoc_success = 0
[ 15.976573] num_cmd_assoc_failure = 0
[ 15.980255] num_cons_assoc_failure = 0
[ 15.984036] cmd_resp_received=0
[ 15.987193] event_received=0
[ 15.990088] max_tx_buf_size=2048
[ 15.993336] tx_buf_size=1536
[ 15.996224] curr_tx_buf_size=1536
[ 15.999556] data_sent=0 cmd_sent=1
[ 16.002971] ps_mode=0 ps_state=0
[ 16.006260] wakeup_dev_req=0 wakeup_tries=0 wakeup_timeout=0
[ 16.011993] hs_configured=0 hs_activated=0
[ 16.016123] pps_uapsd_mode=0 sleep_pd=0
[ 16.019989] tx_lock_flag = 0
[ 16.022896] scan_processing = 0
[ 16.026065] bypass_pkt_count=0
[ 16.029137] mp_rd_bitmap=0x0 curr_rd_port=0x0
[ 16.033517] mp_wr_bitmap=0xffffffff curr_wr_port=0x0
[ 16.038506] mp_data_port_mask = 0xffffffff
[ 16.042623] last_recv_rd_bitmap=0x0 mp_invalid_update=1
[ 16.047867] last_recv_wr_bitmap=0xffffffff last_mp_index=0
[ 16.053369] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.059751] 0x00
[ 16.059754] 0x00
[ 16.061704] 0x00
[ 16.063629] 0x00
[ 16.065574] 0x00
[ 16.067504] 0x00
[ 16.069446] 0x00
[ 16.071369] 0x00
[ 16.073302] 0x00
[ 16.075227] 0x00
[ 16.077169] 0x00
[ 16.079094] 0x00
[ 16.081036] 0x00
[ 16.082958] 0x00
[ 16.084893] 0x00
[ 16.086818] 0x00
[ 16.088756]
[ 16.092170] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.098543] 0x00
[ 16.098546] 0x00
[ 16.100473] 0x00
[ 16.102425] 0x00
[ 16.104356] 0x00
[ 16.106290] 0x00
[ 16.108212] 0x00
[ 16.110146] 0x00
[ 16.112071] 0x00
[ 16.114006] 0x00
[ 16.115929] 0x00
[ 16.117871] 0x00
[ 16.119793] 0x00
[ 16.121725] 0x00
[ 16.123650] 0x00
[ 16.125584] 0x00
[ 16.127509]
[ 16.130943] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.137315] 0x00
[ 16.137317] 0x00
[ 16.139245] 0x00
[ 16.141181] 0x00
[ 16.143105] 0x00
[ 16.145045] 0x00
[ 16.146970] 0x00
[ 16.148912] 0x00
[ 16.150835] 0x00
[ 16.152774] 0x00
[ 16.154700] 0x00
[ 16.156656] 0x00
[ 16.158583] 0x00
[ 16.160504] 0x00
[ 16.162446] 0x00
[ 16.164371] 0x00
[ 16.166309]
[ 16.169740] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.176128] 0x00
[ 16.176131] 0x00
[ 16.178102] 0x00
[ 16.180032] 0x00
[ 16.181967] 0x00
[ 16.183892] 0x00
[ 16.185855] 0x00
[ 16.187783] 0x00
[ 16.189735] 0x00
[ 16.191666] 0x00
[ 16.193611] 0x00
[ 16.195541] 0x00
[ 16.197482] 0x00
[ 16.199406] 0x00
[ 16.201336] 0x00
[ 16.203263] 0x00
[ 16.205193]
[ 16.208627] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.215003] 0x00
[ 16.215006] 0x00
[ 16.216939] 0x00
[ 16.218865] 0x00
[ 16.220799] 0x00
[ 16.222724] 0x00
[ 16.224663] 0x00
[ 16.226589] 0x00
[ 16.228517] 0x00
[ 16.230453] 0x00
[ 16.232383] 0x00
[ 16.234318] 0x00
[ 16.236243] 0x00
[ 16.238182] 0x00
[ 16.240106] 0x00
[ 16.242041] 0x00
[ 16.243964]
[ 16.247392] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.253763] 0x00
[ 16.253765] 0x00
[ 16.255694] 0x00
[ 16.257635] 0x00
[ 16.259558] 0x00
[ 16.261492] 0x00
[ 16.263415] 0x00
[ 16.265349] 0x00
[ 16.267274] 0x00
[ 16.269217] 0x00
[ 16.271148] 0x00
[ 16.273087] 0x00
[ 16.275015] 0x00
[ 16.276987] 0x00
[ 16.278948] 0x00
[ 16.280896] 0x00
[ 16.282823]
[ 16.286252] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.292624] 0x00
[ 16.292626] 0x00
[ 16.294551] 0x00
[ 16.296470] 0x00
[ 16.298405] 0x00
[ 16.300329] 0x00
[ 16.302276] 0x00
[ 16.304205] 0x00
[ 16.306152] 0x00
[ 16.308078] 0x00
[ 16.310013] 0x00
[ 16.311935] 0x00
[ 16.313869] 0x00
[ 16.315793] 0x00
[ 16.317722] 0x00
[ 16.319651] 0x00
[ 16.321592]
[ 16.325051] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.331447] 0x00
[ 16.331450] 0x00
[ 16.333387] 0x00
[ 16.335314] 0x00
[ 16.337259] 0x00
[ 16.339189] 0x00
[ 16.341134] 0x00
[ 16.343062] 0x00
[ 16.344998] 0x00
[ 16.346929] 0x00
[ 16.348893] 0x00
[ 16.350819] 0x00
[ 16.352750] 0x00
[ 16.354678] 0x00
[ 16.356618] 0x00
[ 16.358544] 0x00
[ 16.360471]
[ 16.363899] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.370274] 0x00
[ 16.370277] 0x00
[ 16.372200] 0x00
[ 16.374134] 0x00
[ 16.376057] 0x00
[ 16.377991] 0x00
[ 16.379914] 0x00
[ 16.381846] 0x00
[ 16.383772] 0x00
[ 16.385704] 0x00
[ 16.387629] 0x00
[ 16.389576] 0x00
[ 16.391507] 0x00
[ 16.393450] 0x00
[ 16.395380] 0x00
[ 16.397319] 0x00
[ 16.399244]
[ 16.402670] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[ 16.409039] 0x00
[ 16.409041] 0x00
[ 16.410965] 0x00
[ 16.412911] 0x00
[ 16.414840] 0x00
[ 16.416784] 0x00
[ 16.418713] 0x00
[ 16.420662] 0x00
[ 16.422588] 0x00
[ 16.424507] 0x00
[ 16.426443] 0x00
[ 16.428366] 0x00
[ 16.430321] 0x00
[ 16.432263] 0x00
[ 16.434219] 0x00
[ 16.436141] 0x00
[ 16.438082]
[ 16.441504] bss_index = 0, tx_pkts_queued = 0
[ 16.445879] bss_index = 1, tx_pkts_queued = 0
[ 16.450258] bss_index = 2, tx_pkts_queued = 0
[ 16.454660] bss_index = 3, tx_pkts_queued = 0
[ 16.459045] -------- Dump info End---------
[ 16.463259] Driver version = SD8987----16.92.10.p208-MM5X16292.p4-GPL-(FP92)
[ 16.470426] main_state = 4
[ 16.473145] ioctl_pending = 1
[ 16.476113] tx_pending = 0
[ 16.478886] wmm_tx_pending[0] = 0
[ 16.482254] wmm_tx_pending[1] = 0
[ 16.485585] wmm_tx_pending[2] = 0
[ 16.488915] wmm_tx_pending[3] = 0
[ 16.492227] rx_pending = 0
[ 16.494947] lock_count = 79
[ 16.497755] malloc_count = 55
[ 16.500737] mbufalloc_count = 0
[ 16.503878] hs_skip_count = 0
[ 16.506865] hs_force_count = 0
[ 16.509942] Media state = "Disconnected"
[ 16.513882] carrier off
[ 16.516328] tx queue 0: stopped
[ 16.519493] tx queue 1: stopped
[ 16.522662] tx queue 2: stopped
[ 16.525817] tx queue 3: stopped
[ 16.528969] wlan0: num_tx_timeout = 0
[ 16.532645] wlan1: num_tx_timeout = 0
[ 16.536310] p2p0: num_tx_timeout = 0
[ 16.539936] Start to process hanging
[ 16.543614] Cancel all pending cmd!
[ 16.547147] IOCTL failed: 000000001c9017d7 id=0xe0000, sub_id=0xe0001 action=1, status_code=0x80000007
[ 16.557622] usbcore: registered new interface driver usbxxx
[ 16.589030] wlan: Register to Bus Driver Done
[ 16.593709] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00
[ 16.600102] SDIO Func1 (0x10-0x17): 00 00 00 00 ff ff ff ff
[ 16.606256] SDIO Func1: (0x8) c3 (0x58) 00 (0x5c) 48 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a)
00
[ 16.655851] SDIO Func1 (0xe8-0xf2): dc fe e3 00 9f 00 3f 22 22 01 70
[ 16.792876] SDIO Func1 (0xe8-0xf2): dc fe f1 00 ad 00 3f 22 22 01 70
[ 16.804355] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 16.815310] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 16.821991] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 16.915121] mx8-img-md: Unregistered all entities
[ 17.250788] read descriptors
[ 17.314456] read strings
[ 18.852951] type=1400 audit(1662782903.520:11): avc: denied { setattr } for comm="init" name="dhcp" dev="mmcblk1p9" ino=130599 scontext=u:r:vendor_in
it:s0 tcontext=u:object_r:dhcp_data_file:s0 tclass=dir permissive=1
[ 19.131181] type=1400 audit(1662782910.016:12): avc: denied { read } for comm="composer@2.3-se" name="u:object_r:default_prop:s0" dev="tmpfs" ino=897
3 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.156059] type=1400 audit(1662782910.016:12): avc: denied { read } for comm="composer@2.3-se" name="u:object_r:default_prop:s0" dev="tmpfs" ino=897
3 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.190743] type=1400 audit(1662782910.016:13): avc: denied { open } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:s0"
dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.216477] type=1400 audit(1662782910.016:13): avc: denied { open } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:s0"
dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.241401] type=1400 audit(1662782910.016:14): avc: denied { getattr } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:
s0" dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.266826] type=1400 audit(1662782910.016:14): avc: denied { getattr } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:
s0" dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 19.296476] type=1400 audit(1662782910.016:15): avc: denied { map } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:s0"
dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 20.784740] init: Received control message 'start' for 'bootanim' from pid: 344 (/system/bin/surfaceflinger)
[ 20.796405] init: starting service 'bootanim'...
[ 23.852192] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 25.780968] type=1400 audit(1662782910.016:15): avc: denied { map } for comm="composer@2.3-se" path="/dev/__properties__/u:object_r:default_prop:s0"
dev="tmpfs" ino=8973 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:default_prop:s0 tclass=file permissive=1
[ 25.806587] type=1400 audit(1662782916.944:16): avc: denied { write } for comm="composer@2.3-se" name="brightness" dev="sysfs" ino=43140 scontext=u:r
:hal_graphics_composer_default:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=1
[ 29.345219] init: Received control message 'start' for 'idmap2d' from pid: 501 (system_server)
[ 29.717964] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 29.727462] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 30.217197] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/init.rc:812)
[ 30.437277] init: Received control message 'interface_start' for 'android.hardware.oemlock@1.0::IOemLock/default' from pid: 200 (/system/bin/hwservic
emanager)
[ 30.460856] init: Could not find 'android.hardware.oemlock@1.0::IOemLock/default' for ctl.interface_start
[ 31.369768] read descriptors
[ 31.372734] read strings
[ 31.375469] read descriptors
[ 31.378410] read strings
[ 31.415299] acc_open
[ 31.417620] acc_release
[ 31.868728] Generic PHY 5b040000.ethernet-1:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
[ 31.881812] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 31.917556] mx8-img-md: Registered mxc_isi.4.capture as /dev/video4
[ 31.952924] mx8-img-md: Can't find i2c client device for ov5640_mipi@3c
[ 31.969941] mx8-img-md: Unregistered all entities
[ 35.976789] can-stby: disabling
[ 39.673717] init: Received control message 'stop' for 'idmap2d' from pid: 501 (system_server)
[ 39.697523] init: Sending signal 9 to service 'idmap2d' (pid 361) process group...
[ 39.728019] libprocessgroup: Successfully killed process cgroup uid 1000 pid 361 in 17ms
[ 39.739066] init: Service 'idmap2d' (pid 361) received signal 9
[ 42.636812] init: Service 'bootanim' (pid 491) exited with status 0
[ 42.871365] sdcardfs version 2.0
[ 42.875126] sdcardfs: dev_name -> /data/media
[ 42.879825] sdcardfs: gid=1015,mask=6
[ 42.884738] init: processing action (sys.boot_completed=1) from (/init.rc:803)
[ 42.892861] sdcardfs: mounted on top of /data/media type ext4
[ 42.900365] init: starting service 'exec 13 (/bin/rm -rf /data/per_boot)'...
[ 42.921911] init: SVC_EXEC service 'exec 13 (/bin/rm -rf /data/per_boot)' pid 999 (uid 1000 gid 1000+0 context default) started; waiting...
[ 42.959357] init: Command 'exec - system system -- /bin/rm -rf /data/per_boot' action=sys.boot_completed=1 (/init.rc:806) took 59ms and succeeded
[ 43.014142] init: Received control message 'start' for 'adbd' from pid: 501 (system_server)
[ 43.023802] type=1400 audit(1662782916.944:16): avc: denied { write } for comm="composer@2.3-se" name="brightness" dev="sysfs" ino=43140 scontext=u:r
:hal_graphics_composer_default:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=1
[ 43.089312] type=1400 audit(1662782934.188:17): avc: granted { read } for comm="main" name="u:object_r:net_dns_prop:s0" dev="tmpfs" ino=9028 scontext
=u:r:untrusted_app_25:s0:c512,c768 tcontext=u:object_r:net_dns_prop:s0 tclass=file app=com.android.deskclock
[ 51.878548] type=1400 audit(1662782934.188:17): avc: granted { read } for comm="main" name="u:object_r:net_dns_prop:s0" dev="tmpfs" ino=9028 scontext
=u:r:untrusted_app_25:s0:c512,c768 tcontext=u:object_r:net_dns_prop:s0 tclass=file app=com.android.deskclock
[ 51.901980] type=1400 audit(1662782943.044:18): avc: denied { write } for comm="composer@2.3-se" name="brightness" dev="sysfs" ino=43140 scontext=u:r
:hal_graphics_composer_default:s0 tcontext=u:object_r:sysfs:s0 tclass=file permissive=1
[ 52.306168] init: Received control message 'start' for 'gsid' from pid: 501 (system_server)
[ 52.315138] init: starting service 'gsid'...
[ 53.390615] init: Received control message 'stop' for 'gsid' from pid: 501 (system_server)
[ 54.399015] init: Sending signal 9 to service 'gsid' (pid 1325) process group...
[ 55.412353] libprocessgroup: Successfully killed process cgroup uid 0 pid 1325 in 5ms
su
Module Size Used by
g_serial 16384 0
hci_uart 53248 0
moal 720896 2
mlan 471040 1 moal
mek_8q:/ # ifconfig -a
wlan0 Link encap:Ethernet HWaddr 00:13:cb:71:ba:00 Driver wlan_sdio
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
eth0 Link encap:Ethernet HWaddr 3a:0c:2c:38:27:14 Driver fec
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
ip_vti0 Link encap:UNSPEC
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
can0 Link encap:UNSPEC Driver flexcan
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 TX bytes:0
Interrupt:82
ip6_vti0 Link encap:UNSPEC
NOARP MTU:1364 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
wlan1 Link encap:Ethernet HWaddr 00:13:cb:71:bb:00 Driver wlan_sdio
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
dummy0 Link encap:Ethernet HWaddr 0e:05:68:b4:ab:49
inet6 addr: fe80::c05:68ff:feb4:ab49/64 Scope: Link
UP BROADCAST RUNNING NOARP MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:700
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope: Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
ip6tnl0 Link encap:UNSPEC
NOARP MTU:1452 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
p2p0 Link encap:Ethernet HWaddr 02:13:cb:71:ba:00 Driver wlan_sdio
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 TX bytes:0
[ 56.422881] init: Service 'gsid' (pid 1325) received signal 9
[ 55.158053] woal_do_scan fails!
[ 56.397555] init: Received control message 'start' for 'gsid' from pid: 545 (system_server)
[ 56.406613] init: starting service 'gsid'...
[ 56.481759] init: Received control message 'stop' for 'gsid' from pid: 545 (system_server)
[ 56.490137] init: Sending signal 9 to service 'gsid' (pid 1388) process group...
[ 56.503362] libprocessgroup: Successfully killed process cgroup uid 0 pid 1388 in 5ms
[ 56.513773] init: Service 'gsid' (pid 1388) received signal 9
[ 60.210755] woal_do_scan fails!
[ 61.318464] woal_do_scan fails!
[ 65.255321] woal_do_scan fails!
[ 70.273399] woal_do_scan fails!
[ 71.265043] woal_do_scan fails!
[ 71.588629] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 72.808512] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 75.291810] woal_do_scan fails!
[ 89.656122] init: Received control message 'interface_start' for 'android.hardware.wifi.hostapd@1.0::IHostapd/default' from pid: 193 (/system/bin/hws
ervicemanager)
[ 89.686144] init: starting service 'hostapd'...
[ 89.961209] capability: warning: `hostapd' uses 32-bit capabilities (legacy support in use)
[ 90.073308] set mac address failed! status=-1, error_code=0x0
[ 90.080012] Set MAC address failed
[ 90.130907] get fw info failed! status=-1, error_code=0x0
[ 90.151209] get fw info failed! status=-1, error_code=0x0
[ 90.157238] Set country code failed!
[ 90.163628] 11D: Error setting domain info in FW
[ 90.169767] 11D: Error setting domain info in FW
[ 90.220491] Uap SCAN failure
[ 90.223619] wlan1: Skip change virtual intf on uap: type=2
[ 90.236480] Uap SCAN failure
[ 90.239599] wlan1: Skip change virtual intf on uap: type=3
[ 90.295114] init: Service 'hostapd' (pid 1530) exited with status 0
Hello,
Could you please help me validate that you are not impacted by the issue in this thread?
Regards
Hi estephania_mart ,
Even after applying the patch using the below thread, cmd53 error is not resolved. https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/uSDHC-auto-tuning-and-possible-SDIO-fail...
Also, We are getting issue related to invalid domain detected which we are suspecting as the root cause for cmd53 error. Kindly comment on this regulatory issue and let me know how to break the deadlock.
Thank you for your early reply.
Hello,
Please, help me check this other post.
Regards