JN5189/K32W: a module made for 20dBm output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5189/K32W: a module made for 20dBm output

JN5189/K32W: a module made for 20dBm output

The High Power board design files can be found on the JN5189 product webpage, in the JN-RD-6054-JN5189 Design Files. More precisely, the reference manual and the design files are attached to this article (OM15072-2_MOD_EXT_AMP_QFN40_PCB2467-2.0.zip and JN-RM-2078-JN5189-Module-Development_1V4.pdf)

Some guidance is available here.

The RF performances are presented in the attached test report (powerpoint file).

The FCC/IC Certificates or Declarations of conformity are in the article "Certificates/Declarations of conformity (nxp community)".

 

附件
100% 有帮助 (1/1)
版本历史
最后更新:
‎08-25-2021 05:54 AM
更新人: