Hi Guys
I'm using Processor Expert 10.4 to configure a Vybrid
Problem I have is that when I select pin B14 for I2C0 SCL, the tool also checks pins K18 and L3 (which I need for other things) -see attachment
i2C1 behaves as I would expect (I can select any one of the available pins)
Is this a bug in the tool, or is there some strange dependency in the chip I'm not aware of ?
Solved! Go to Solution.
Hi,
I have the same behavior as Vilem.
The version I have is the next:
I wonder if there is any difference. I am not sure if there is an update package you need.
The installation details are the next:
Regards,
Alejandro
Hi Alejandro & Vilem
Thanks for your reply :smileyhappy:
It looks like there is a later version of PE - I will check
In the meantime, since I was still able to change my hardware design, I changed from I2C0 to I2C1, which does not have any issue
Regards
Alan