For the Vybrid platform there is the linux user space program "mqxboot" which allows to load and start an M4 image. I have a short test application for M4 which is using MQX and looks like this:
void main_task ( )
{
puts ("hello from M4");
while (1)
{
// do nothing else
}
}
When I load the image with mqxboot, everything is fine and I see the expected string on stdout. But when I try to load the image a second or third time the output is not done anymore, so I assume that the M4 application is still running from the first mqxboot-call.
Question: Is there an option to explicitely stop the M4 application and reload a new/other application?
Thanks,
Johannes
解決済! 解決策の投稿を見る。
Hello Johannes,
When the Vybrid resets, the M4 clock is disabled. What the mqxboot utility does is it loads an MQX program into memory and releases the M4 clock, so the M4 core starts executing.
There is no way to reset the M4 core without resetting the A5, so there is no way to start a new program on the M4.
Thanks, and let me know if you have any questions.
Timesys Support
By writing 0x05fa0001 into 0xe000ed0c (VECTRESET of AIRCR) I was able to reset M4 and restart MQX while A5 is still running and unaffected.
Pato,
Can you please provide the page number in the Vybrid Reference Manual where this "AIRCR" register is described? PDF search for that term returned nothing. Thanks.
I made a new video of my stuff and this pretty neat M4 reset feature is at 04:45
https://www.youtube.com/watch?v=Prykiy97e34&feature=youtube_gdata
When doing a Debug-Stop, the Crossworks toolchain invoques a Javascript which does the M4 reset:
function DebugEndCM4()
{
TargetInterface.pokeWord(0xe000ed0c, 0x05fa0001); // VECTRESET
}
This doesn't seem to work. I tried it with the 2N02G mask Vybrid. It looks like just a memory location as I can read back what I wrote.
I wonder if there's a way to poke that word in DS-5....
Have you tried asking ARM ?
That's what I did with Crossworks, thinking that this feature might be useful to others as well.
Hi Jack,
Unfortunately there is no single source of infos and it's all scattered around. From my experience of the past 4 or 5 months with this MCU, the Vybrid Reference Manual is just the starting point, then the ARM site is the next place to check out (but no fun at all with tons of documentations, revisions, infos relevant or not to the Vybrid)...
Regarding the AIRCR, I found what I was looking for in Joseph Yiu's definitive guide to the ARM Cortex-M3 second edition Table 7.4 on page 113:
- VECTRESET Resets the Cortex-M3 processor (except debug logic), but this will not reset circuits outside the processor
which does exactly what I want.
Thanks for that reference. I'll have to get that book. I also found this about the AIRCR on ARM's website:
Interesting, thanks Jack. So far writing 1 to VECTRESET has been working fine for me but it's good to know ARM recommends writing 0 instead.
Can you try writing zero to that bit and see if that works, too? I have a feeling that they're not mentioning something.
You're right, writing 0 doesn't work!
They said:
"When writing to the register you must write 0 to this bit, otherwise behavior is Unpredictable."
I think that "Unpredictable" behavior when writing a '1' to this bit is that it causes a reset to that core and only that core.
Hello Johannes,
Only one M4 application being loaded per Linux session is supported. In order to reload your M4 application, you will need to reset your board.
Thanks, and let me know if you have any questions.
Timesys Support
Hi,
thanks for the reply! But I'm still wondering if there is no other option to restart the M4 from A5 side? Maybe I can modify the mqxboot application in any way?
Thanks,
Johannes
Hello Johannes,
When the Vybrid resets, the M4 clock is disabled. What the mqxboot utility does is it loads an MQX program into memory and releases the M4 clock, so the M4 core starts executing.
There is no way to reset the M4 core without resetting the A5, so there is no way to start a new program on the M4.
Thanks, and let me know if you have any questions.
Timesys Support
timesyssupport can you help on this case?