Vybrid VG Graphics - Spinning Tiger Demo on Auto EVB w/MQX GC355

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid VG Graphics - Spinning Tiger Demo on Auto EVB w/MQX GC355

Jump to solution
6,143 Views
billkrakar
NXP Employee
NXP Employee

Discussion area for partners and alpha customers who are working to get VG graphics going on Vybrid.

The intent is for this discussion to be populated by the Freescale internal team with the latest files, instructions, tips etc. to allow others to create a known working platform with the Spinning Tiger Demo running on the Auto EVB Rev C w/ MQX 4.0.2 and the MQX VG drivers (0.4.0 now and 0.5.0 shortly) using HW acceleration on the GC355 GPU.

0 Kudos
Reply
1 Solution
4,806 Views
ioseph_martinez
NXP Employee
NXP Employee

I added the uboot sources to the same extranet site http://freescale.com/livelink/livelink?func=ll&objid=226470266&objAction=browse&sort=name

In the tar file there is a binary if you want to skip the building process.

View solution in original post

0 Kudos
Reply
24 Replies
437 Views
jasonwilliamson
Contributor II

Do you know if this procedure works with microSDHC cards, or is a pure microSD card required?

0 Kudos
Reply
437 Views
ioseph_martinez
NXP Employee
NXP Employee

Yep, it also works with SDHC, I just have here a working 4GB SDHC.

437 Views
dirkdoerr
Contributor III

I was able to build MQX following the instructions.

It might be worth mentioning that I failed using a more recent version of the Windows Sourcery toolchain. After switching to Linux using the matching toolchain version I could build it.

But I failed building the tiger example:

I couldn't apply the patch. It failed with hunk #15 failed error message.

In the lists of include directories I see this:

$(GC3XX_ROOT)/hal/os/$(OS_TYPE)/inc


I couldn't find a matching directory.


Maybe I am using the wrong version of "vf600 OpenVG 0.4.0". I got mine from the Freescale compass extranet

0 Kudos
Reply
437 Views
dirkdoerr
Contributor III

Short update:

I used a wrong mqx path.

Now I can compile the demo

0 Kudos
Reply