Processor expert project for the Vybrid Tower board TWR-VF65GS10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor expert project for the Vybrid Tower board TWR-VF65GS10

跳至解决方案
2,398 次查看
adiroot
Contributor I

Is there a Processor Expert sample project for the Vybrid Tower board TWR-VF65GS10?

标签 (2)
0 项奖励
回复
1 解答
1,546 次查看
timesyssupport
Senior Contributor II

As Jack has said, it does not appear that the VF6xx PEx projects are available at this time. You may use them as a guideline to build your own PEx project for the Vybrid.

Thanks,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,543 次查看
harshadlele
Contributor II

Hi,

I am curious, are the VF6xx PEx projects are available now?

if yes then can someone point me out to them.

Thanks in advance.

0 项奖励
回复
1,546 次查看
jackblather
Senior Contributor I

Look here: Where can I find Processor Expert examples and tutorials in Driver Suite?

If you're using Linux as a development host, go to this directory:

~/.ds-5/workbench/ProcessorExpert/Projects/TWR-VF65GS10

I'm using Processor Expert on the TWR-VF65GS10.

0 项奖励
回复
1,546 次查看
adiroot
Contributor I

Thanks Jack.  However, despite the fact that the folder is called TWR-VF65GS10, those projects are not for that tower!. 

The example projects all call out to the SVF512R3MK4 CPU.  The TWR-VF65GS10 tower board has the VF61GS151CMK50 CPU on it.

0 项奖励
回复
1,546 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help with this case?

0 项奖励
回复
1,546 次查看
timesyssupport
Senior Contributor II

Using the Microcontrollers Driver Suite v10.3 plug-in for existing Eclipse via the following link:

PE_DRIVER_SUITE: Processor Expert Software, Microcontroller Driver Suite

We can confirm that the SVF512R3MK4 CPU is used for projects under ~/.ds-5/workbench/ProcessorExpert/Projects/TWR-VF65GS10. jackblather have you used these sample projects with the Vybrid Tower? Do you know why the CPU for these projects differs from that which is on the tower?

Thanks,

Timesys Support

1,546 次查看
jackblather
Senior Contributor I

I suspect that these examples were based on the VF5xx parts instead of the VF6xx because when these examples were created, the VF6xx parts may not have been available yet. The dates on the example PEx-Generated code is Feb 27, 2013.

I imported those examples into my Workspace in DS-5 (Ubuntu), but I am not able to build it - those examples are targeted for the IAR tool chain on Windows. However, I used them as examples to build my own PEx project. They were useful because they allowed me to see how the parameters of the components are configured etc.

0 项奖励
回复
1,546 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you continue with the follow up?

0 项奖励
回复
1,547 次查看
timesyssupport
Senior Contributor II

As Jack has said, it does not appear that the VF6xx PEx projects are available at this time. You may use them as a guideline to build your own PEx project for the Vybrid.

Thanks,

Timesys Support

0 项奖励
回复