Hello,
I'm porting old timesys BSP to the new Yocto Jethro, we use a 7" LCD panel with egalax touch screen device (like i.MX6 sabre design).
We use the freescale egalax driver with bindings in device tree :
&i2c0 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c0>;
status = "okay";
at24@50{
compatible ="at24,24c08";
pagesize = <16>;
reg = <0x50>;
};
touchscreen: egalax_ts@04 {
compatible = "eeti,egalax_ts";
reg = <0x04>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eeti2>;
interrupt-parent = <&gpio0>;
interrupts = <21 0>;
wakeup-gpios = <&gpio0 21 GPIO_ACTIVE_LOW>;
};
};
pinctrl_eeti2: eeti2grp {
fsl,pins = <
VF610_PAD_PTA31__GPIO_21 0x063f
>;
};
and PTA13 is used as IRQ pin (GPIO 21)
When booting, egalax driver is registered, but it can't set irq, see bootlog in attached file.
Any suggestions?
Regards
Emmanuel
Original Attachment has been moved to: bootlog.txt.zip
Solved! Go to Solution.
Hello,
I did similar workaround with the 3.0 kernel. I found a solution for the 4.1 kernel, but don't ask me what was the real problem.
I just rewrote the end of egalax_ts_probe, see attached diff file.
It works, but with ts_test, cursor is a little bit jerky due to time out error in I2c reading, but it should be fine for my application.
Thanks,
Emmanuel
timesyssupport please continue with the follow up.
Hello,
I made some test with GPIO Sysfs interface, and it seems to work
16: 25654 GIC 27 Edge gt 17: 0 vf610-gpc 8 Edge eDMA tx 18: 0 vf610-gpc 9 Edge eDMA err 19: 0 vf610-gpc 4 Edge SEMA4 21: 3050 vf610-gpc 62 Edge fsl-lpuart 32: 0 vf610-gpc 30 Edge fsl-dcu-fb 33: 422216 vf610-gpc 71 Edge 40066000.i2c 34: 0 vf610-gpc 92 Edge wkpu-vf610 35: 0 vf610-gpc 75 Edge 40034000.usb 37: 0 vf610-gpc 100 Edge rtc alarm 38: 3054 vf610-gpc 76 Edge 400b4000.usb 39: 2244 vf610-gpc 78 Edge 400d0000.ethernet 40: 8 vf610-gpc 83 Edge vf610_nfc 63: 38510 gpio-vf610 21 Level egalax_ts 125: 51 gpio-vf610 19 Edge gpiolib
Now I think that it could be an interrupt mask problem, because with IRQF_TRIGGER_LOW (level trigger), interrupt is permanently triggered (counter grow up quickly) , if I replace by IRQF_TRIGGER_FALLING (edge trigger), interrupt is never triggered.
I think it's not really an IRQ conflict, because I tried to force an other IRQ number (125 for example), and the problem remain the same.
Regards,
Emmanuel
Hi Emmanuel,
So, I inquired with one of our Vybrid developers about this, and turns out we did work with an egalax touchscreen for another partner's Vybrid platform, but in the 3.0 kernel. They initially saw a similar issue as you are currently seeing in 4.1 - so many interrupts were being generated with IRQF_TRIGGER_LOW that this was causing a large system slowdown. We changed the driver to use falling edge interrupt instead - please see the attached patch to do so. You could investigate porting the changes from this patch to your 4.1 kernel egalax driver.
Also, sorry about the length of the patch, most of the changes are whitespace changes rather than content changes. You should be able to ignore code line #s ~100-185 in the patch.
Thanks,
Timesys Support
Hello,
I did similar workaround with the 3.0 kernel. I found a solution for the 4.1 kernel, but don't ask me what was the real problem.
I just rewrote the end of egalax_ts_probe, see attached diff file.
It works, but with ts_test, cursor is a little bit jerky due to time out error in I2c reading, but it should be fine for my application.
Thanks,
Emmanuel
timesyssupport please continue with the follow up.
Hello,
The egalax_ts is well probed, because egalax driver is registered :
input: EETI eGalax Touch Screen as /devices/platform/soc/soc:aips-bus@40000000/40066000.i2c/i2c-0/0-0004/input/input0
in egalax_ts_probe :
error = devm_request_threaded_irq(&client->dev, client->irq, NULL,egalax_ts_interrupt, IRQF_TRIGGER_LOW | IRQF_ONESHOT, "egalax_ts", ts);
if (error < 0) { dev_err(&client->dev, "Failed to register interrupt\n"); return error; }
didn't return errors.
I think the problem is not egalax_ts driver.
Weird, I just tried with Toradex kernel 4.1, and it works.....
I will make a diff....
Thanks ,
Emmanuel
Hello,
Somebody can explain how interrupts numbers are attributed, because irq number is already defined before enter devm_request_threaded_irq, client->irq is 60.
with linux-3.0.13, egalax interrupt number was 277, but many things changed since linux 3.0 .....
Regards,
Emmanuel
Hi Emmanuel,
This is likely due to the introduction of the ARM GIC driver for Linux kernel >3.0, which is assigning a different virtual interrupt number in the newer kernel.
Thanks,
Timesys Support
timesyssupport can you help to review this case?
Hi Emmanuel,
I could see irq 60 from your boot log which is GIC id for SDHC1.Could you please confirm your kernel version and complete boot log along with the output of "cat /proc/interrupts" ?
Thanks,
Timesys Support
Hello Emmanuel,
We have reviewed your device tree configuration , but have not found anything wrong with this. We are not able to reproduce your issue because we do not have the egalax hardware with the vybrid tower, so you will need to debug the driver in the 4.1 kernel at drivers/input/touchscreen/egalax_ts.c.
If you had this working in the previous bsp then I would recommend reviewing the probe function in that egalax driver compared to the probe function in the egalax driver in the 4.1 kernel.
Thanks,
Timesys Support
Hello,
I made some tests with Toradex kernel, and it doesn't work, there's also irq conflict, what cause asynchronous reads of egalax device. Even when IRQ line is in idle state, the isr routine is called, then ts_test works but very slow.
I tried to use PTA30 as irq line (instead of PTA31), the problem still there with IRQ 62 (DCU 0). It seems something is broken in irq management.
In 3.0.15-ts-armv7l, cat /proc/interrupts gives :
277: | 61 | GPIO egalax_ts |
Regards,
Emmanuel