Trace on Vybrid with DS-5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace on Vybrid with DS-5

1,316件の閲覧回数
hjk
Contributor III


I am now using TWR-VF65SG10 Tower Board , and I can boot from SD card, by the way I am on windows host

I'm trying to use DS-5 to trace on this board, and I follow the step as follow link

https://www.google.com.tw/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0ahUKEwjmk7Sfs...

here's one step

"Plug in an Ethernet and connect it to your local PC. The board is set to static IP of 169.254.0.100. Set your PC to something similar like 169.254.0.1."

so I unplug my host ethernet cable, and use crossover cable to connect the target board and my host(windows)

but the ip address showed from the A5 is 192.168.1.3  so I changed the IP addr to it

"Adjust the host’s networking so that it can communicate with the target. TCP/IP (for example Ethernet) is used to communicate with the target when doing application level debug and Streamline profiling"

I change my host (win7) IP address to 192.168.1.1 and default gateway to 192.168.1.254

but it didn't work

I was wondering where did it go wrong,

0 件の賞賛
返信
3 返答(返信)

1,093件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

You are correct.

Closed this  thread and  follow up continues in the other thread.

0 件の賞賛
返信

1,093件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 件の賞賛
返信

1,093件の閲覧回数
timesyssupport
Senior Contributor II

Hi Karina,

This appears to be a duplicate of the following request:

https://community.freescale.com/message/633843?et=notification.mention#comment-633843

Thanks,

Timesys Support

0 件の賞賛
返信