From MQX to Baremetal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

From MQX to Baremetal

1,003 次查看
SlaveToTime
Contributor II

Hi,

I'm trying to do something complicated.

I have code written for Crossworks,a Baremetal project for M4.

I don't need,and probably it should be only a complication, to use MQX.

The only problem with this is that the MCC and examples,are written only for LINUX(A5)/MQX(M4), or MQX(A5)/MQX(M4).

I am only interested to not change the MCC part on linux,if it is possible,but only the MQX part of MCC.

Do you think that it is possible and not so complex?

What's the best way in your opinion?

标签 (5)
标记 (2)
0 项奖励
回复
2 回复数

690 次查看
timesyssupport
Senior Contributor II

Hello Alessandro,

It should be possible to port MCC to another RTOS; however, I cannot say the exact amount of time it would take, as Timesys has not used the Crossworks baremetal project.

We would imagine the MCC sources for MQX would be the best starting point. These are located in your MQX installation directory, at mcc/source/.

We also have an MCC User Guide available at the following location, which has more information about the MCC API and implementation:

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc

Thanks,

Timesys Support.

690 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help to attend this case?

0 项奖励
回复