CMIS-DSP on Vybrid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CMIS-DSP on Vybrid

跳至解决方案
1,137 次查看
carlovalgocela
Contributor III

Hello

I have read CMSIS-DSP library in Freescale (http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf).

I would like to know if this is supported in Vybrid VF6xxx

As what i read on the document, examples are for Kinetis.

What libraries do i need to add.

Current setup:

- DS5 v5.19

- OS (Ubuntu 14 and Windows 7)

- Freescale MQX 4.0.2

标签 (3)
0 项奖励
回复
1 解答
904 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
905 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
907 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi Carlo,

As you can see in the app note in IAR only a check box and a header found in the IAR folder installation are needed. But you can download the package from arm http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.p...

Please notice that the libraries are only for Cortex M4.

0 项奖励
回复