Hello
I have read CMSIS-DSP library in Freescale (http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4489.pdf).
I would like to know if this is supported in Vybrid VF6xxx
As what i read on the document, examples are for Kinetis.
What libraries do i need to add.
Current setup:
- DS5 v5.19
- OS (Ubuntu 14 and Windows 7)
- Freescale MQX 4.0.2
解決済! 解決策の投稿を見る。
元の投稿で解決策を見る
Hi Carlo,
As you can see in the app note in IAR only a check box and a header found in the IAR folder installation are needed. But you can download the package from arm http://www.arm.com/products/processors/cortex-m/cortex-microcontroller-software-interface-standard.p...
Please notice that the libraries are only for Cortex M4.