ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ラベル

ディスカッション

ソート順:
Depending on which MCU Devlopment board you have chosen, you will need to figure out a way to mount this to the chassis. I have seen everything from cardboard, to aluminum, to wood. Below is a template complete with CAD drawings to mount the Qorivva TRK-MPC5604B board and the Motor Board onto the chassis. We use plexiglass for ours, but any other millable material is appropriate. The large hole in the middle is for cables from the servo. We attach the board to the car using the plastic standoffs (you will need them 55 mm long, so in our case, we used the combination of 40 + 15 mm) - see an example (SOS code 10260). To attach both the processor and interface boards the simillar 5mm plastic standoffs were used. Preview (.pdf) CAD file (.dxf)
記事全体を表示
Video on YouTube done by the University of Applied Sciences of Munich about the Freescale Cup event held on March 18th Freescale Cup 2014 an der Hochschule München - YouTube
記事全体を表示
Students from the University Applied Sciences TDU Deggendorf gave yesterday a demonstration of their Freescale Cup cars. 10 teams had worked during the semester in getting their cars running on their homemade Freescale Cup track based on Tower K60 kits. They ran them with lights on, lights off, in both directions on the track. Solid performance overall. HDU Deggendorf's teams are led by Prof. Gerald Kupris and have enrolled for the 3rd consecutive season into the Freescale Cup EMEA Challenge 2014. They are preparing another set of cars to compete in the upcoming racing season.
記事全体を表示
The TWR-K40X256 Kit is a Freescale evaluation board powered by the Kinetis K40 microcontroller. The Kinetis microcontroller family is a set of 32 bit ARM Cortex M4 chips which feature flexible storage, lower power usage, high performance and optional Floating Point Unit with many useful peripherals. For more information on the Kinetis family see Freescale's Kinetis website. The Tower System is a prototyping platform with interchangeable and reusable modules along with open source design files. TWR K40X256 Hardware Setup There are several main hardware configuration steps. After installing the battery, once the USB cable has been connected between the evaluation board and PC, it may be necessary to update the chip firmware which requires moving a jumper pin on the evaluation board. TWR K40X246 Hardware Setup Instructions Board Specific Tutorials K40 Blink LED K40 Drive DC Motor K40 Drive Servo Motor K40 Line Scan Camera Board Tips The TWR-K40X256 features a socket that can accept a variety of different Tower Plug-in modules featuring sensors, RF transceivers, and more. The General Purpose TWRPI socket provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Table 3 of the TWR-K40X256 User's Manual, but the user manual does not describe how to order a connector A Samtec connector, part number: SFC-110-T2-L-D-A is the proper female mating connector for the TWR-K40X256 TWRPI socket. SIDE A/SIDE B White DOTS for counting Pins Solder Wire to GND, and to MCU VDD Pin for testing purposes Important Documents TWR-K40X256 User's Manual TWR-K40X256 Schematics External Links TWR-K40X256-KIT Webpage Kinetis Discussion Forum Tower Geeks Community Website Tower Geeks Freescale Cup Group
記事全体を表示
Second part in the series showing tips and tricks to getting the most of your line scan camera.
記事全体を表示
Couple of new videos. This time I am running the FRDM-TFC library demo code written by Eli Hughes without any change at all-- successfully on my car. I have had the 0 ohm R24 res replaced with a higher one thanks to the soldering skills of David DiCarlo! The first video highlights demo modes 0 through 3: Car demos - YouTube Demo 0- test buttons and switches Demo 1- test servo Demo 2- test motors Second, I was able to get my little o-scope (xprotolab) to capture the camera analog out-- here: Camera testing - YouTube No major coding done but I understand the library and ports on the boards much better now.   Still haven't resolved the 'whining' apparent when I enable the H-bridge but I will try a few things this week-- it is possible it is harmless. Next steps, buffering camera data then on to control loops! Daniel Oh, I was also able to get the serial port working while code was running so I could get some dynamic feedback. This document was generated from the following discussion: Videos testing out Freescale Cup kit
記事全体を表示
The Team from the University of Padova in Vicenza are working in getting their race car ready for the upcoming EMEA Finals that will be held in Paris on 26-27 March. They filed this short video on a make up track. Conditions were not the best so they had to scale down the speed.
記事全体を表示
2013 Global Freescale Cup Participant: USA Car Specs: -Custom motor driving circuitry -FRDM-KL25Z -Dual line scan camera Related Videos             
記事全体を表示
2013 Global Freescale Cup Participant: Brazil Car Specs: -Freescale "Bolero" MPC5604B 32-bit MCU
記事全体を表示
2013 Global Freescale Cup Participant from Mexico Car Specs: -Freescale "Bolero" TRK-MPC5604B
記事全体を表示
2013 Global Freescale Cup Participant: Malaysia Car Specs: -Freescale Freedom FRDM-KL25Z
記事全体を表示
How to setup GPIO on the Kinetis. Includes discussion on enabled clocks to peripherals and setting up the pin control registers.
記事全体を表示
Discussion of how to setup interrupts on the NVIC. The Flex timer is used as an example
記事全体を表示
2013 Global Freescale Cup Participant: Japan Car Specs: -Freescale "Bolero" MPC5604B 32-bit MCU
記事全体を表示
Clock setup on the Kwikstik
記事全体を表示
Qorivva Based Freescale Cup Webinars:  Lecture 1: Introduction and Motor Basics Lecture 2: Pulse Width Modulation Lecture 3: Control Design Lecture 4: Speed and Position Lecture 5: MPC5607B Overview
記事全体を表示
The Fraunhofer Institute of Integrated Circuits in Erlangen (Germany) is the inventor (with Thomson) of the MP3 files most of use today in our smartphone and media players. They are over 20,000 researchers strong and a force in the R&D community in Germany and around the world. The institute will welcome and host the Freescale Cup 2014 EMEA finals on 29-30 April 2014. It is a great chance for the student teams that will be at the event to get a glimpse of engineering R&D at its best and make contact with talented Fraunhofer Institute engineers shaping the world of tomorrow. See the press release at 20130715_Freescale_2014 - Fraunhofer Institute for Integrated Circuits IIS
記事全体を表示
2013 Global Freescale Cup Participant: India Car Specs: -Freescale "Bolero" MPC5604B 32-bit MCU
記事全体を表示
'''Topics we want to cover''' Advanced Components Accelerometer Gyro Ultra-sonic Temperature Humidity Pressure GPS Power Efficiency Modes Serial I/O SD Card Terminal Debugger Bluetooth Wifi RF - Zigbee Capacitive Touch Memory Data Logging Graphics Segmented Display TFT DSP CMSIS A/D conversion Advanced Motor Control Three Phase Motor Control Motor Synchronization
記事全体を表示
Kinetis Header Part 2 of 2
記事全体を表示